Other Parts Discussed in Thread: TPS84A20 I have an application which looks perfect for the TPS84A20, except the output voltage required is +6V. From the equation, it looks like a value of 159 ohms would set it to 6V. With the higher output voltage, the…
Other Parts Discussed in Thread: TPS84A20 I have a question regarding simultaneous sequencing on the TPS84A20 where the output of one TPS84A20 tracks another one. I have been following the process that is recommended in the TPS84A20 data sheet on page 24…
Hello Kent,
TPS84A20 is 100% compatible with LMZ31710.
You may also want to consider LMZ22010 , LMZ12010 , PTH08T241W , PTH08T240W .
I am not an expert in supply chain issues, so I will refrain from trying to explain the reason for the shortage.
Happy holidays…
Other Parts Discussed in Thread: TPS84A20 For CAD library, I need urgently information for TPS84A20 dimensions and location of the exposed thermal pad.
This information is not given in the datasheet
Part Number: LMZ31520 Other Parts Discussed in Thread: TPS84A20
Hello
I don't find the MTBF Data (LMZ31520 & TPS84A20)
Please Can you Send to me the MTBF Data of this Device?
Regards.
Other Parts Discussed in Thread: TPS84A20 , TPS84259 Hello,
We need power module of below conditions.
----------------
Vin:+10V
Vout:-5V
Iout:3A
----------------
There is inverting application note as below.
http://www.ti.com/lit/an/snva425a/snva425a…
Other Parts Discussed in Thread: TPS84A20 Hi,
We are planning to use the TPS84A20 power supply in our prototype design. In the datasheet, No dimension details for the Exposed Thermal Pins(41 & 42).
Please send it to us ASAP to create Footprint.
…
Hello Arrigo san,
Thank you fo the reply.
Cable length : about 100mm at both of Vout / GND.
Model :PLZ164WL ( this model can set 25A/us of slew rate)
I measured transient responce of 5A/us of TPS84A20 by this constitution.
So I think that TPS84259 indactance…
HI Sir / madam ,
Vengad here from Avnet , one of my customer is using below part for new proejct .
LMZ22005 & TPS84A20 . It is possible to get the IBIS Model ?
Regards/
Vengad
Hi Tony,
We have other parts that can be put in parralel for higher current. If you can give me a list of the voltages and currents in your designs we could look for other solutions.
For Example the TPS84A20 is a current sharing 10 amp module, that is…