Part Number: TPS922055 Other Parts Discussed in Thread: LM3409 , LP8865Z-Q1
Hi,
We have designed a led driver using the TPS922055, it will drive a led string with 6 leds at 2A maximum for use with machine vision. We chose the TPS922055 because of…
Part Number: TPS922055 Tool/software: The TPS922055 Calculation tool (TPS92205x_Cal_Tool_V1p2_preview_version.xlsm) give either 10uH or 22uH values for the inductor required, based soley in switching frequency. Is this appropriate or should one follow…
Part Number: TPS922055 Other Parts Discussed in Thread: TPS92641 ,
Tool/software:
Hi,
How can I request the latest SIMPLIS models of the following two parts?
TPS922055 and TPS92641
Currently the TPS922055DMTREVM is out of stock, so we urgent…
Part Number: TPS922055 Tool/software: Hi,
Is it possible/ advisable to parallel two TPS922055 devices to increase the current drive available.
I know there is an option of going to an external FET but these devices work very well and we appreciate…
Part Number: TPS922055 Tool/software: Hello,
I'm using TPS922055 in the design to drive the LEDs, Setting the maximum LED current to 2.4A by using a 0.082 ohm sense resistor.
But when I powered the board and measured the output current, I got…
Part Number: TPS922055 Hi,
I need to design a cost-effective, low BOM, and power-efficient circuit based on the TPS922052DRRR (3A) or TPS922055DRRR (6A).
The 6A part seems like the better choice since low thermal impact is required. The requirements…
Part Number: TPS922055 Tool/software: Hi team,
1. Does the TPS922055 work with 200kHz switching frequency, and dimming PWM is 20kHz. Is it able to have the output current PWM rising time and falling time shorter than 2us? I saw the user guide of EVM…
Part Number: TPS922055 I'm looking for a simple circuit using TPS922055 chips to control LED lighting in a vision system.
The goal is to control the TPS922055 via an ESP32 to create pulses during camera exposure.
I also need to be able to change the…
Part Number: TPS922055 Other Parts Discussed in Thread: TPS92640 , TPS92641 Tool/software: Hi,
I’m seeking a deeper understanding of the TPS922055 and its internal workings in my specific application. Here's the setup:
Input Voltage (Vin) : 48V…