Part Number: TPS922055 Tool/software: Dear TI Forum,
a week ago, we received a TPS922055DRRREVM evaluation module in a WSON package. However, the components on this module differ from those listed in the TPS92205xEVM Bill of Materials.
Could you provide…
Part Number: TPS922055
Tool/software:
Dear TI-,
I 'm writing to request a review of my design. The project specifications are as follows:
The LED driver will be driving 3 LED @0.7A, connected in series (with 3*Vf = 3*12V).
Vcc = 48V
Switching…
Other Parts Discussed in Thread: TPS922055 Tool/software: What is the start-up timing for the FAULT pin?
From were in time does it have a valid state?
Could I use the FAULT function to power down the device? But then for how long do I have to mask…
Part Number: TPS922055 Tool/software: Hi.
I'm currently working with the TPS922055 EVM board and noticed some unexpected behavior related to PWM dimming:
When I gradually increase the duty cycle as shown in the attached examples, the LED stays off…
Part Number: TPS922055 Other Parts Discussed in Thread: TPS92518HV , LMR36500 Tool/software: Hi,
i am searching for an adjustable power supply in the range of:
Input voltage: +48V (fixed)
Output voltage of about +12V to +32V @0,5mA max.
The…
Part Number: TPS922055 Tool/software: Dear TI,
I would like to request a review of the following design. The goals of the design are as follows:
Dimming of 12x Cree XP-G4 High Intensity LEDs in series
42V input
Hybrid dimming (ADIM/HD pulled…
Part Number: TPS922055 Tool/software: Hi,
we are using the TPS922055 for the first time und unfortunately ran into some issues with it:
Expected behavior: - Quadratic increase of LED current up to set current (606 mA) with flexible dimming Observed…
Part Number: TPS922055 Hello guys,
One of my customers is considering using TPS922055 for their next products as a light source for camera.
They want to drive LED current, 5A as the maximum with 256 steps. At this moment, they have the following questions…
Part Number: TPS922055 Other Parts Discussed in Thread: TPS92640 , TPS92641 Tool/software: Hi,
I'm looking for an alternative to the TPS922055 (but similar functionality) that can handle a higher input voltage in the range of 65V to 70V. In my application…
Part Number: TPS922055 Tool/software: Hi,
I have an IC that I am trying to identify. It is marked with the following: P2055 TI318 A3C2
I've done some preliminary research, however, I haven't been able to find a definitive datasheet or more…