Hi Philipp,
Philipp D said: However, it seems that these are not sufficient to disable sleep mode right after startup. At first trigger it takes about 5ms to reach the desired 1A LED current. From the second trigger on rise time is about 20us.
Is this…
Hi Kazuya,
Please refer to my comments below:
If the customer wants to accelerate the soft-start (around 5 ms) time, they can use flexible dimming in the way shown in this E2E FAQ - [FAQ] How to get a quick transition of TPS922055 / TPS922054 / TPS922053…
Hi Dave,
Dave Kearney said: Hi, I have implemented the TPS922054DRRR driver in a circuit as below. It is driving 2x Cree XTEAWT-E0-0000-00000BKE1 LEDs in parallel . Vf of each LED is 2.77V. I have it set to drive the LEDs at 3A (no dimming required), providing…
Tool/software: Hi Teams,
I would like to know about the design of the UVP resistor divider.
In the following thread, it was mentioned that the design should ensure the voltage is above 1.4V.
[FAQ] How to design the UVP resistor divider for TPS922055…
Part Number: LP8868W-Q1 Other Parts Discussed in Thread: TPS922055 , Hello Experts, The calculation formula of L in datasheet p22, I think this is typo. I suppose TPS922055 datasheet is correct. Would you check it, please? - LP8868W-Q1 - TPS922055 Best Regards…
Part Number: TPS922055DMTREVM Other Parts Discussed in Thread: TPS922055 Hi Team,
Use TPS922055 driver LED lamp, 36V power, output voltage 20-25V, current 3.5A.
Use the oscilloscope to check the chip 14 pin SW, when the PWM is less than 10%, the output…
Hi Tonu,
Please refer to this E2E FAQ - [FAQ] How to design the UVP resistor divider for TPS922055 / TPS922054 / TPS922053 / TPS922052? - Power management forum - Power management - TI E2E support forums .
Tonu Arulaane said: It was said that UVP pin has…
Part Number: TPS923655 Other Parts Discussed in Thread: TPS922055 , TPS922054 Hello, I have a question.
I'm currently trying to turn on a 12V LED using a Li-ion battery with 3 series.
Conditions to be used 1. Vin = 8V~12.6V 2. Vled = 12V 3. Iled = 2.…