Part Number: TPS92210 Other Parts Discussed in Thread: PMP6023 Hi,
I noted that the 0-10V dimming ratio is 9:1. what does this mean?
are there many methods of 0-10V dimming or is it always an isolated interface using an opto-coupler to transfer the signal…
Part Number: TPS92210 Other Parts Discussed in Thread: TPS92075 , PMP4347 , TPS92314 Hello
Thank you for your cooperation usually.
Customer think TPS92210 (PMP3672) seems good solution for their next project.
Customer changed spec to follow PMP3672 as per…
Hi Craig,
The simplest PFC that can work with this low voltage and power would be the UCC28056 . However, this may not be able to hit your THD target. The UCC28180 is a CCM PFC which might be a better choice to optimize for low THD. Neither of these is…
Part Number: TPS92210 Hi Support team,
My customer found a reference design PMP5652 using TPS92210, but their output current needs to be doubled of PMP5652. Is TPS92210 still applicable for their design? Here is the spec requirements:
- Input voltage…
Part Number: TPS92210 Hello,
I would like ask a few questions about NATURAL PFC LED LIGHTING DRIVER CONTROLLER.
I need to drive 10-12 350mA power leds for a traffic light application so I want to know if this LED driver is good enough.
Firstly, I want…
Hello Rajesh,
Thank you very much for your interest in TPS92210, I would like to direct you towards the design calculator tool attached. Please have a scroll and have a quick check if your spec matches the recommended values.
PMP6023 can be a good starting…
Part Number: TPS92210 Hi, i was trying to do a power supply (12V@0,5A) with a Buck Configuration.
But here is the issue: Doesn't work when my input is equal to 220V. At 127V works ok.
There is a trouble with DZ3, the voltage never reachs to 5v1, then…
Part Number: TPS92210 Dear Sir,
We designed PCB for Constant output Voltage and constant current 9W LED driver. The following are the 9W LED driver specifications:
Specification:
Input
Operating Voltage Range
120 to 270 VAC
Operating Frequency…
Part Number: TPS92210 Hi,
Specification:
Input
Operating Voltage Range
120 to 270 VAC
Operating Frequency Range
48 to 62Hz
Power factor
>0.95
Harmonic Distortion (THD)
<12%
Isolation
Isolated input and output ground…