Part Number: TPS92314A Other Parts Discussed in Thread: TPS92314 , TPS92210
Hello
I found that TI has 4 reference designs for T8 tube with TPS92314A.
For universal ( AC85-265) design, PMP4347 seems good reference, but
do you have non-isolated reference…
Part Number: TPS92314A Other Parts Discussed in Thread: TPS92314
Hello
My customer intend to choose TPS92314 for next T8 tube project.
*Vin AC 85 ~265V
*Vout=70V ;VF=2.4V x 28pcs => VF=67.2V
*T8 size 280 mmx 18mmx 8mm ( therefore, PMP4347
seems to…
Part Number: TPS92314A Other Parts Discussed in Thread: TPS92075 , TPS92074 , TPS92560 , LM3445 Hello guys,
One of my customers is looking for a AC/DC LED driver IC has 15~35W capavility and PFC. I reccommended them TPS92314A. Their answer was that the device…
Part Number: TPS92314A Other Parts Discussed in Thread: PMP6024 , UCC28810 , LM3447 , TPS92210 I need to design a small size, isolated 50W LED driver. The purpose of this project is to replace an existent driver. I have many led panels in warehouse with…
Part Number: TPS92314A Other Parts Discussed in Thread: TPS92314
Hello
Do you have test data of IEC61000-3-2 for TPS92314 EVMs or TI Design like as PMP4362?
I think it should be have by customer themselves, but it is necessary to select TPS92314 by customer…
Dear Irwin, Thanks for the prompt reply. yes you may have to add some external circuitry to kill this problem. This may be a better approach than adding the more elaborate low voltage cutoff circuitry. I will be grateful if you can come up with some idea…
Other Parts Discussed in Thread: TPS92314A Dear All,
I m an newbie to designing
I just happen to start designing TPS92314A IC The First problem I found was with the sample calculations provided in the datasheet, the Numerical answer are an little out…
Hi, I want to know the input surge withstand capacity of this design - PMP7672.
Also how to ensure that this design can withstand 10KV surge ?
Regards
Atul Bhakay
Other Parts Discussed in Thread: TPS92314A Dear Sir, We are currently using TPS92314A in our street light solutions both 40W and 60W(60Vx600mA, 60Vx900mA). Is it possible to extend the power ouput to 80W960Vx1200mA)? Please confirm with changes if any…