Part Number: TPS92380 Hi team,
Background: In the TPS92380 datasheet (Fig. 9-4, p28), L1 is shown as a single inductor in SEPIC mode. For SEPIC topologies, L1 is generally implemented either as a coupled inductor or as two separate inductors.
Questions…
Part Number: TPS92380 Hello guys,
One of my customers is evaluating TPS92380.
At this moment, they have the following question. Could you please give me your reply?
Q. TPS92380 datasheet says "Alternatively, a T-divider can be used if resistance…
Part Number: TPS92380 Tool/software: Can you send me the link of a mounting constraints of TPS92380PWPR? I want temperature, limit number for mounting and so on.
Part Number: TPS92380 Hello guys,
One of my customers is evaluating TPS92380 for their new products.
At this moment, they have the following question. Could you please give me your reply?
Q. Depending on the customer power sequence, the PWM pin…
Part Number: TPS92380 Other Parts Discussed in Thread: TPS92360 Tool/software: Hello guys,
One of my customers is evaluating TPS92380 using the SEPIC circuit shown on page 28, Figure 9-4 of the datasheet. At this moment, they have the following questions…
Part Number: TPS92380 Tool/software: I designed a board with TPS92380 mounted on it, but I found that when combined with the LCD, some combinations have the backlight on and some do not. I have confirmed that there is no damage to the LCD or the board…
Part Number: TPS92380 Hi E2E support team,
Is there a hardware star-up sequence that TPS92380 must follow?
I found sequence in the datasheet, Are the 500us delay required?
I need to consider adding delays(TPS3897A) and load switch to the schematic…
Part Number: TPS92380 Hi E2E team,
The block diagram is as follows:
The backlight characteristics of the panel are as follows:
Here are my design value calculations and schematic.
Calculation for TPS 92380 Parameters Design.xlsx
My choice…
Part Number: TPS92380 Other Parts Discussed in Thread: LP8869-Q1 The EVM specified for the TPS92380 appears to be the same board as for LP8869-Q1.
Are these in effect the same device? For a basic functional test can the standard build of the EVM be…