Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Hi Leven,
Yes, TPS61196 or TPS92391 both can combine the FBx to support large current LED strings.
TPS92391 data sheet, product information and support | TI.com
BR
Patrick
Part Number: TPS92391
Hi,
My design (using the TPS92391) has a potential situation whereby during system shutdown, battery voltage (3-4.2V) may be present on the power input to the LED driver (so present at the VSENSE_N and VSENSE_P pins) , but the VDD…
Part Number: TPS92391 Section 7.3.8.5 Hybrid Mode of the TPS92391 datasheet, at the bottom of Page 25, states that:
"The PWM and current modes transition threshold can be set at 12.5% or at 0% brightness. The latter selection allows for pure current…
Hi Gary,
The current per channel is max 50mA. If you want 100mA /CH, please refer to below device.
TPS92391 Boost/SEPIC High Dimming Performance LED Driver with Six 200-mA Channels datasheet (ti.com)
BR
Patrick
Hi David,
I think you can consider our TPS92390/TPS92391 which have 4ch/6ch with 200mA max per channel.
And may I know what's the EE of customer?
TPS92390/TPS92391
BR
Patrick
Part Number: TPS92390 Other Parts Discussed in Thread: TPS92391 If Vin is 24V and assuming that LED string short-circuit is not possible, is it possible to have Vout higher than 48V, e.g. up to 70V? Same question for TPS92391.
Part Number: TPS92381 Other Parts Discussed in Thread: TPS61177 , TPS61196 , TPS92391 Dear Team,
Do we have any suitable solution can meet below backlight led spec?
Many Thanks,
Jimmy
Part Number: TPS61160 Other Parts Discussed in Thread: TPS61161 , TPS92391 Hi Team,
Could you check the max operation current for TPS61160?
Many Thanks,
Jimmy