Part Number: TPS92511 Other Parts Discussed in Thread: TPS92640 Hello guys,
One of my customers is considerring using TPS92511.
But the device output current accuracy is lower a littel bit than their requirement.
They need +/-5% current accuracy…
Part Number: TPS92511 hi. Respected engineers.
1. tps92511 is not a calculator document? Required.
2. Is low brightness control related to inductor value when analog dimming?
Part Number: TPS92511 Dear Specialists,
My customer'd like to know when ILED is 40mA.
I would be grateful if you could advise.
---
Since it is necessary to set the LED current consumption to about 40mA due to the system current consumption, I…
Part Number: TPS92511 Evaluating the TPS92511 LED driver for incorporation into a new product. This device will not simulate within Pspice . I sent the .lib file to Cadence to see if they had the same problem with it, and their tech said that it is missing…
Part Number: TPS92511 Hi all,
I try to use the TPS92511 within an application with 6V-36V input voltage. The LED current should be 50mA. The choosen inductor is 220mH (Murata 45224C). The R_iadj ist 30K. R_FS is 30k as well. The current ist 42mA@6V…
Part Number: TPS92511 Other Parts Discussed in Thread: LM3466 Hi
Can TPS92511 be used with 12 paralleled LEDs?
If yes, what potential risk it will have?
Part Number: TPS92511 Dear Specialists,
My customer'd like to know the LED Current accuracy at RIADJ=30kohm and RIADJ=38kohm.
The datasheet P.5 Electrical Characteristics ILED only described RIADJ=3kohm, 6kohm and 10kohm.
Could you please let us…
Part Number: TPS92511 Other Parts Discussed in Thread: TPS92692 , TPS92691 , INA149 Hello guys,
One of my customers is looking for a device which external MOSFET version of TPS92511. If the switching MOSFET is external, it can be used for higher voltage…
Part Number: TPS92511
Hi,
I am facing the issue of an occasional MOSFET failure on the TPS92511. I am driving an 5 LED Strings with each their own TPS92511 and PWM. They are supplied from a common 48V power supply with an additional PI-Filter. The…
Part Number: TPS92511 Hi TI Team,
We need a constant current of 500 mA for a string of LEDs with dimming functionality for a 7inch TFT LCD.
Nominal input voltage is 12V.
LED forward voltage is in the range of 8.7 V to 10.5 V.
Please suggest…