Part Number: TPS92512HV Tool/software: This Part no-TPS92512HV
My requirement layout and inbuild ic.
1.Input voltage -40v
2.Seriase led -12, Led voltage-3.3
3.Output current -2.5amp
Part Number: TPS92512HV Tool/software: Hi,
I am using the TPS92512HV in a system where power is controlled by an interlock mechanism:
Power is disconnected when the interlock is triggered.
Power is reconnected when the interlock is released. …
Part Number: TPS92512HV Tool/software: Hi,
We use the TPS92512HV for our LED driver, and now, the Inductor howl issue is happen when the output current is larger than 0.7A, our input voltage is 12V and output current is 2.5A max.
Pleaes refer to below…
Part Number: TPS92512HV Other Parts Discussed in Thread: TPS92512 , TPS922055
Hi there,
We design a led drive board with TPS92512HV with design parameters as below:
min
max
Typical
Vin
22V
26V
24V
Vout
3.7V…
Part Number: TPS92512HV Other Parts Discussed in Thread: TPS92515HV , TPS92515 Hello,
I have a request to dimmer 48V LED board using constant voltage drivers with pwm output (for example meanwell-pwm series that works at 1.47kHz or others slower drivers…
Part Number: TPS92512HV Other Parts Discussed in Thread: TPS92512 Hello,
I have designed LED driver circuit using TPS92512. My requirement is to drive LED with constant current of 535mA at the minimum input of 44V (Typical:48V).
I have LED's with…
Part Number: TPS92512HV Dear Sir/Ms.
My customer asked me if the action of TPS92512HV OTP is whether the chip temperature reaches 165 degrees, it will be turned off directly (100%→0%), or the current will decrease proportionally (100%→??%→??%→0%) What…
Part Number: TPS92512HV Hi team,
Posting this question for my customer as it may be beneficial to others that have a similar question.
Thanks for the help!
"We understand the TPS92512HV driver has a temperature shut off mechanism that works autonomously…
Other Parts Discussed in Thread: TPS92512HV , TPS92512 , TPS92513 Hello team,
Customer is needing to drive a single 1A (3W) LED with 2.5-3V working voltage and considering TPS92512HV for constant current source and PWM dimming. Would we have any other…