Part Number: TPS92513HV Dear Sir,
My customer want to use TPS92153HV for 48Vin, 1.5A Iout application to driver 8 SFH4715AS. Is there any design guide for customer's reference? Or anything they have to take care? Thermal pad design or? Thanks for your…
Part Number: TPS92513HV I build a circuit for LED driver using TPS92513HV. The circuit is same as the typical application in datasheet, just different at output current. The input current stays at same level when I increase the input voltage. But I measured…
Part Number: TPS92513HV Hello guys ,
we are using tps92513Hv IC in DC to Dc driver.
our products specifications input 54V and output 50V/1A . when we are given supply to the buck input ,after that if we are removing and connecting (O/P port) to the load…
Part Number: TPS92513HV Hi all,
We designed a LED driver based on TPS92513HV.
Input: 48V, 3.3V PWM signal.
Output: 30V max, 1A.
Schematic attached
. led-driver.pdf
In green - current sense out after LPF. this signal go to MCU.
In yellow - LED output…
Part Number: TPS92513HV In my design supply input voltage and required LED driver output is same(36V)
In design calculation difference between Vin - Vout is zero and inductor value becomes zero, Duty cycle is also '1'
kindly support on this d…
Part Number: TPS92513HV Other Parts Discussed in Thread: TPS92512 , TPS92513 Hi team,
The problem is that output waveform is not stable. When they configure output frequency to 130kHz with Vin 56V, Vout 48V, 1A load and no PWM dimming, the duty cycle varies…
Hello Cees,
I haven’t heard back from you, I’m assuming you were able to resolve your issue. If not, just post a reply below (or create a new thread if the thread has locked due to time-out)
Best Regards,
Part Number: TPS92513HV Other Parts Discussed in Thread: TPS92512 , TPS92513 , LM3409 , TPS92640 , TPS92515 Customer wants to use 4 TPS92513HV to implement 4 parallel output for LED driver application, with 1A for each output. Could you please help check whether…
Part Number: TPS92513HV Other Parts Discussed in Thread: TPS92513 , TPS92512 Hi,
I downloaded TPS92513 SPICE model and created a symbol for it. But this is encrypted and not running in the simulation.
Can you please help me with the SPICE model?
Thanks, …
Part Number: TPS92513HV Other Parts Discussed in Thread: TPS92513 Hello guys,
One of my customer considering using TPS92513 for their net products.
They want to know how many LED in series can be byTPS92513 drive with 60V input and 500mA current?
Could…