Part Number: TPS92513HV Other Parts Discussed in Thread: TIDA-01096 , CC2650 , TIDA-01095 , CC2540 Hi Team,
TIDA-01096 didn't include the SW sample code, please suggest where to find it? thanks.
www.ti.com/.../TIDA-01096
Part Number: TPS92513HV Hi,
We have a LED drivers design where 3 LEDs are powered at 450mA and we are breaking all the prototypes we are testing.
This is the original design where some values have been changed:
The C15 value is now of 10uF and R9 is…
Part Number: TPS92513HV E2e Support,
We have a field issue where the PDIM pin (5V max) of this IC was connected to 48V through a 68K resistor. This is 700uA through the ESD diode in the IC.
What is the max current rating of that diode?
Thanks for…
Part Number: TPS92513HV Hi,
We got a question from the customer about TPS92513HV. Could you help us?
[Question] They are considering using the IC at following condition.
Vin=50V Vout=3V Iout=1A
They are concerned about the minimum on time and the power dissipation…
Part Number: TPS92513HV The LED current should be selected by the switching between 8 different resistors. Because of space constrains an additional LDO should be avoided and therefor the usage of the 500mV coming from the RT/CLK pin as suggested in the…
Part Number: TPS92513HV Other Parts Discussed in Thread: TPS92515 , TPS92513 , Hello i am a german engineer an i will use the device above with many LED from the same type on the same String (connected all LEDs in one line)
For this i will use 60VDC as voltage…
Part Number: TPS92513HV Other Parts Discussed in Thread: LM3447 , TPS92314 , TPS92075 , TPS92074 , LM3444 Hi SIr/Madam,
My customer have below requirement for LED driver design. Please advise if TPS92513HV is the correct part to propose. If there is reference…
Part Number: TPS92513 Other Parts Discussed in Thread: TPS92515 , , TPS92512HV , , TPS92512 I have to design PCB with 3 LED drivers with 48V powers supply, normal current will be selected later between 0.5 and 1A. All drivers will be controlled with PWM…
Part Number: TPS92513EVM-001 Other Parts Discussed in Thread: TPS92513HV , TPS92513 Hello E2E,
Could you please guide us how to modify TPS92513EVM-001 to support 54Vin?
Except changing TPS92513 to TPS92513HV, anything else need to modify?
BR,
Jason