Part Number: TPS92515HVEVM-749 Tool/software: Hi. Although other posts give a link to product page, there are no PCB files.
Are they available for the Evaluation module? Thank you.
Part Number: TPS92515HVEVM-749 Other Parts Discussed in Thread: TPS92515HV , TIDA-01081 , CSD18543Q3A
Hello,
I’m designing a board to control some LED (12x, in series).
I’m using the TPS92515HV to do so. I have used a transistor to short the LEDs…
In item 1, can you confirm 2 LEDs in series given through J3, not J2?
In item 3, It shows that LED current is on/off, which means VLED+ changes with some kind of control; The LED current you measured is not 2A, just around 100mA. While according to…
Part Number: TPS92515HVEVM-749 Other Parts Discussed in Thread: TPS92515 Hello,
I have tried to connect PWM (after having set the right jumpers) and it damaged the board.
Any insights?
Thanks.
Sana
Part Number: TPS92515HVEVM-749 Other Parts Discussed in Thread: TPS92515 Hi,
I am trying to use a TPS92515HVEVM board to control a LED COB.
ILED max 700mA and LED Vf: 35V, Vin = 50V ,PWM dim, 2kHz signal from a MCU.
I use the TPS 92515 Design Calculator…
Part Number: TPS92515HVEVM-749 Other Parts Discussed in Thread: TPS92515 , LM3405 , LM3410 , TPS92513 , TPS92515HV I'm looking for a device to driver single LED in range of 350~900mA with continuous wave. Input voltage 5V.
Is TPS92515 with analog dimming…
Part Number: TPS92515HVEVM-749 Dear TI,
I have TPS92515HVEVM-749 High Current buck LED Driver Evaluation Module. I see that ILED can be set with Jumper J1. For my purpose I need to replace Jumper with Switch/Analog MUX or Micro Solid State Relay with…
Part Number: TPS92515HVEVM-749 Other Parts Discussed in Thread: TPS92515HV hi sir
I want to use the TPS92515HV to driver the led module
could you help me to deisgn the circuit? dc 24v/0.72w
thanks
thanks
Part Number: TPS92515HVEVM-749 Hi Team,
My customer now use TPS92525-EVM to test.
The Vin is 12V and output is 2.08V with about 100mA camera load.
Customer removed the R14 resistor on the EVM board and connected it to the PWM control terminal of…
Part Number: TPS92515HVEVM-749 Other Parts Discussed in Thread: TPS92515 Hello E2E,
I seted the Vadj to 0-V(GND) for stop the ILED completely. However LEDs are lighting. Please let me know how to stop the ILED. (without shunt-FET using)
Regards, …