Part Number: TPS92515HVEVM-749 Other Parts Discussed in Thread: TPS92515 Dear support team
Seeing at TPS92515EVM, it is possible to charge Coff from Vcc through R7, but what are the advantages of this configuration? Is there a merit of charging from Vcc…
Part Number: TPS92515HVEVM-749 Hello all,
Where would I find the design files for schematic and design files for TPS92515HVEVM-749 ?
There is no link for downloading the files in previous posts.
Thanks!
Regards,
Elena Aparicio
Part Number: TPS92515HVEVM-749 Dear TI,
I did some test of your EvalBoard and LED current on 1 Ohm resistor looks not good. I used Vin= 26 V and PWM= 5V (continually). With 1.5A resistor divider setup I see only glitches till 1.7A and current goes back…
Part Number: TPS92515HVEVM-749 Other Parts Discussed in Thread: TPS92515HV I have a TPS92515HV evaluation board that I am using to control a strobe light. The strobe is intended to have a 50% duty cycle, requires about 34V output, and 1.3A. I am powering…
Part Number: TPS92515HVEVM-749 Hi All,
The SW waveform when TPS92515HVEVM-749 is operated without load is as follows.
Vin=12V
I think the reason why SW is falling is because HisideSW is turned off.
Is it correct?
What is the timing to turn it ON again…
Part Number: TPS92515HVEVM-749
Greetings!
I have been evaluating the TPS92515HVEVM-749. I modified the circuit to do Shunt PWM and analog dimming accordingly to datasheet (put diode, resistor, and pot). However, when I did the shunt FET, I could see…
Part Number: TPS92515HVEVM-749 Hello team,
Hope you are well. Where would I find the design files for schematic and design files for TPS92515HVEVM-749?
Schematic and layout are both displayed in the user's guide SLVUAR5-May 2016 but there is no link for…
Part Number: TPS92515
Hi support team,
I input the voltage divided by the resistor to the IADJ terminal. Is there a recommended resistance value range?
Please let me know the usable range.
The TPS92515HVEVM-749 uses 38.3kohm to 100kohm.
Regards, Dice-…
Hello~
When we design with DCDC IC,what parameter related to inductor and FET we should check? For inductor , the Isat,Irms,DCR........?And how to check it , just check oscilloscope figure , EMC and heat?
And I learnt tps92515HVEVM-749 schematic from…