Part Number: TPS92518EVM-878 Greetings,
Table 4, page 15 of SLUUBM0A lists C16 & C21 of having a rating of 16V, Should these not be rated for at least 60V?
If no, what is the justification?
thanks
Part Number: TPS92518EVM-878 Other Parts Discussed in Thread: LM3409 , TPS92518 Can TI provide scope plots of current responses of an LED string using PWM diming and shunt-FET dimming? The turn-on and turn-off times using PWM diming as well as the current…
Part Number: TPS92518EVM-878
Information:
Worked initially
No fault on GUI
VCC2 = 7.45V with drive enabled/disabled
May have accidentally connected external PWM(3V) signal to SW2(TP5)
Any suggestions of other things to check or try?
Part Number: TPS92518EVM-878 Other Parts Discussed in Thread: TPS92518 I recently requested and received a TPS92518 EVM however i cannot find a link to download this software anywhere on its page or in the mysecure software section
Part Number: TPS92518EVM-878 I am in need of a footprint for the evaluation board and a simulation model for the evm board and its companion board for use in alitum. Please help.
Part Number: TPS92518HV-Q1 Other Parts Discussed in Thread: TPS92518EVM-878 , LEDSPIMCUEVM-879 Hi,
We are working on a new design for an existing LED controller product.
We are very interested in seeing if the TPS92518HV-Q1 would be an effective replacement…
Part Number: TPS92518EVM-878 Hello again TI,
My strobing application requires the shunt FET circuitry to minimize the inductor current rise/fall-times for short LED on-times
1) Why was the TPS92518EVM-878 not provisioned with the shunt FET circuitry and…
Part Number: TPS92518EVM-878 Hello TI,
1) Is it possible to obtain the gerber files for the TPS92518EVM-878? I need to modify the board for my application and would like to re-print on 11X17 with a white background for my technician with redlined annotations…
Part Number: TPS92518EVM-878 Hello,
TPS92518EVM-878 Board layout, Fig 14, pg 12, SLUUBM0A, appears to show provision for two current sense resistors in parallel for each channel, yet the schematic does not show this. 1) Are there provision for qty 2,…
Part Number: TPS92518EVM-878 Other Parts Discussed in Thread: TPS92518 Hi Engineer,
If we would like to demo the TPS92518 EVM without the MCU board and GUI.
Do you know if the SPI pin could be floating or not?
If not, what's the right signal I should give…