Part Number: TPS92518HV Other Parts Discussed in Thread: TPS92518 Hello!
The TPS92518 has an internal LDO generating Vcc (~7.5V) from Vin.
I am able to efficiently generate 7.5V externally, and I would like to use that if possible.
Can I power Vcc…
Part Number: TPS92518HV Other Parts Discussed in Thread: TPS92518 Tool/software:
Hi everyone,
I've run into a critical issue with a new board design that incorporates two TPS92518 LED drivers.
The board and the TPS92518 ICs work perfectly fine under…
Part Number: TPS92518HV Tool/software: Hello E2E Experts,
Good day.
We have a PCB similar to the TPS9518HV evaluation board. A PIC16F1827 MCU supervises 2 TPS9518's for a total of 4 LED channels powered from a 48V supply. Although the PIC can successfully…
Part Number: TPS92518HV Other Parts Discussed in Thread: TPS92518 Tool/software: Hello everyone,
I am trying to write a setup for my TPS92518. I can calculate all registers except the register LEDx_PK_DAC.
According to the illustration (Datasheet…
Part Number: TPS92518HV Other Parts Discussed in Thread: TPS92518 Tool/software: Hi, page 15 of datasheet for TPS92518HVPWPR notes that the IC has a tleb (min on time) that must be considered for every application to avoid a inductor saturation condition…
Part Number: TPS92518EVM-878 Other Parts Discussed in Thread: TPS92518HV , TPS92518 Hello - I'd like to evaluate the TPS92518HV chip to drive a high power LED while still being able to dim to very low outputs. At maximum, our output is about 58V and 5A…
Part Number: TPS92518HV-Q1 Other Parts Discussed in Thread: TPS92518 Hello TI expert,
I met with a technical problem with TPS92518 HV chip. i use this chip to work with TPS92662 , realize matrix function.
when i set up the Tpk =40, Toff=40, the coill…
Part Number: TPS92518HV Other Parts Discussed in Thread: TPS92518 Hi,
we have done a design with 2 altmost identical TPS92518HV (i.e. 4 channels). The design is closely related to the EVM schematic, see below.
When activating the shunt FET, the TPS…
Part Number: TPS92518HV Other Parts Discussed in Thread: TPS92518EVM-878 , LEDSPIMCUEVM-879 , TPS92518 Hi,
I am planning to reduce the idle-consumption of a device. Right now, the VIN pin of the TPS92518HV draws 3-4mA when idling, which is to much for…