Part Number: TPS92518HV Hello,
Is there a way to put the TPS92518HV into a constant voltage output mode?
For example: setting the device to 1 Amp max and it runs the output up to max voltage (in our case 57.5 Volts minus the drop across the output N channel…
Part Number: TPS92518HV-Q1 Other Parts Discussed in Thread: TPS92518 , Hello,
My customer is looking for IBIS model, specifically for SPI, in TPS92518HV-Q1. I did not find it under the Models section of the product page. Can you please provide it? If one…
Part Number: TPS92518HV Hi all, I'm trying to figure out why my driver circuitry based around the TPS92518HV doesn't appear to be producing the output current I have calculated in the design phase.
One of the remaining question marks is around…
Part Number: TPS92518HV-Q1 Tool/software: WEBENCH® Design Tools Hello,
Is there a BXL symbol file available for TPS92518HV-Q1? I could not find it on the product folder or webench.ti.com/cad/ search portal. One of our customers is requesting this.
Thanks…
Part Number: TPS92518HV-Q1 During the use of the TPS92518HV-Q1, the temperature of the IC is measured to be high. I think this is not normal. Please give pointers. Details are as follows:
1. Design parameters
Vin: 48V Vled: 0-37.6V Iled: 0.7A Fsw = 300Kh…
Part Number: TPS92520-Q1 Other Parts Discussed in Thread: TPS92518HV-Q1 , Hello,
Are there efficiency calculator tools available for TPS92520-Q1 and TPS92518HV-Q1? If not, is there an efficiency comparison between these drivers under the same or similar…
Part Number: TPS92518HV Other Parts Discussed in Thread: LM3409HV , LM3409 , TPS92518 Hello,
What happens when the output of the TPS92518HV is shorted to ground? Is it like the LM3409HV where it just delivers the correct current at near zero volts?
I don…
Part Number: TPS92518HV Other Parts Discussed in Thread: TPS92518 There is another behavior I can't figure out.
If the last command to the 92518 was a write (specifically to Toff[MAX]), then at some point after I don't talk to the device, the SPI Error…
Part Number: TPS92518HV Other Parts Discussed in Thread: TPS92518 , LM3409HV , LM3409 Hello.
I have a prototype hardware up and running. Love the part. Love the linearity. I'm making good progress.
In the process of debugging a python test script, I…