Part Number: TPS92612 Hi-All,
I have a question regarding the use of the TPS92612. The customer is using the TPS92612 to drive LEDs via a 3.5m cable. The LEDs are connected in parallel (two LEDs).
1)I understand that connecting LEDs in parallel is…
Part Number: TPS92612 Other Parts Discussed in Thread: LM3404 , Hi team,
My customer is considering an LED driver product for bathroom vanity lighting. The required specifications are as follows:
Linear topology (for noise reduction)
Dimming…
Part Number: TPS92612 Hi,
I bought this part from Aliexpress and the body marking is "1J6F", is there any supplier that also carried the part number TPS92612? Cos the datasheet reference the part marking as " 22SF". If not, what could this body marking…
Part Number: TPS92612-Q1 Other Parts Discussed in Thread: SN6507 , , TPS92629-Q1 , TPS92621-Q1 , TPS92621Q1EVM Hi, my customer is looking to flash an LED (<100mA) at around 50kHz, and vary the duty cycle according to an analogue voltage (NTC).
The available…
Part Number: TPS92612-Q1 Other Parts Discussed in Thread: TPS92612 Hello TI Support,
I want to use the TPS92612 in a design. I would like to run it above 20Khz but lower than 100KHz. Would this be possible to do with the TPS92612.
What are the limitation…
Part Number: TPS92612 Other Parts Discussed in Thread: LP5522 , , TPS92610EVM , Tool/software: Hello,
My customer would like to blink and LED at 0.5Hz (1 second on and one second off). They do not want to use I2C, and would prefer a resistor for setting…
Part Number: TPS92612 Other Parts Discussed in Thread: TPS929120-Q1 , Tool/software: Hey,
Assuming I need to power 10 or more 0.5W LEDs, what would be the best system approach here? Should I use multiple devices, each powering just 2 or 3 LEDs? Any…
Part Number: TPS92612-Q1 Other Parts Discussed in Thread: TPS92612 Tool/software: Hi team,
Customer think of extending the wiring from the board with TPS92612 to an LED installed in another part of the vehicle to drive the LED. (For example, is it necessary…
Part Number: TPS92612 Other Parts Discussed in Thread: TPS92620-Q1 , TPS92621-Q1 , TPS92621Q1EVM Hi team,
I am looking for below device.
VIN is 24V PWM voltage (400Hz, or 1kHz), customer is considering a constant-current output (PWM drive) with an…
Part Number: TPS92612-Q1 Hello Concern,
We are using TPS92612-Q1 in our Application - as we have a requirement of Short to Battery protection.
But when we are shorting the OUT pin to VBAT --> LED Driver got damaged (After Reset Showing the 0.4V…