Part Number: TPS92612-Q1
I need to drive my LEDs with a very low duty, typically 0,1%. With a PWM frequency of 1KHz (1000uS period) and a PWM input of 1uS positive, 999uS Gnd, the LEDs flicker, When I look at the signals, I see that LED output sometimes…
Part Number: TPS92612-Q1 Other Parts Discussed in Thread: TPS92612 , TPS92633 This component appears unobtainable. Lead times I see are 73 weeks. Is this going to improve, or do I just need to design in a replacement part? TI seems to be worse than most…
Part Number: TPS92612-Q1 Other Parts Discussed in Thread: TPS92612 , LM3410 Hi Team.
My customer now use TPS92612-Q1 in charging the NiMH battery.
the input is 8V, the output current need to be 50mA.
Here are two questions about TPS92612:
1/ Whether it will…
Part Number: TPS92612-Q1 The problem is present when a have a low PWM, for a pulse widht under 25uS, independiently of the frequency (100Hz...10KHz).
I have 5 frames exactly equals, and playing with the PWM, at the umbral of LED ON / OFF, the different…
Part Number: TPS92612-Q1 Hi Team,
The customer has configured as below.
Project Spec :
Input voltage: 9V ~ 16V
Output voltage: 9V (LED 3EA Serial x 2)
Output current: up to 20 mA
Q1. Is there no problem if I connect the battery power directly and receive…
Part Number: TPS92612-Q1 Hi, Team,
Customer need to know the max PWM frequency for the PWM pin input. We can't find it in datasheet, could you support it?
Another question: When the 5V input missing, and adding a 12V at the OUT pin, will it damage…
Part Number: TPS92612-Q1 Other Parts Discussed in Thread: TPS92612 Hi Team,
Since the 912 does not have a dedicated EN pin, can the PWM input pin be used as an Enable somehow?
Thanks,
Jared
Part Number: TPS92612-Q1 What is the purpose of the DIODE connected to the power input side in the TPS92612-Q1 application?
What is the effect if there is no diode?
Part Number: TPS92612-Q1 Team,
I would like to know if there is any action could improve the ESD performance of TPS92612-Q1 output pin.
They would like to pass the ISO 10605 +/-15kV for contact and air. I understand this is system level ESD spec. So…