Is there a recommended part number for the zener to use with the TPS92613-Q1?
Obviously, it needs to be 3.3V, but are there any other necessary specifications such as leakage current, etc.?
Thanks.
Part Number: TPS92613-Q1 TI recommends a 200 Hz PWM signal with a 1-100% duty cycle input to control brightness, but what is the upper frequency limit of the PWM signal?
Part Number: TPS92613-Q1 Other Parts Discussed in Thread: TPS929120-Q1 please tell me
Is there a recommended LED driver that meets the following conditions for TI products? -The number of LEDs and forward voltage are unknown because LED-UNIT is used -The…
Part Number: TPS92613-Q1 Other Parts Discussed in Thread: TPS929120-Q1 Greetings,
Is there any recommended LED drivers available in current TI catalog?
-Linear,
-single channel
-current 350 mA
-Low VDrop Perhaps 0.2 V max if possible(I think it's difficult…
Part Number: TL4242-Q1 Other Parts Discussed in Thread: TPS92613-Q1 , , TPS92610-Q1 , TPS92611-Q1 , TPS92612-Q1 Dear all,
Is there any alternative solution for TL4242TDRJRQ1?
Proposing P2P device would be perfect, but any comments on the device that has similar…
I did not mention who I was quoting but it was was Sean Zhou in a thread at: on August 9th.
So, there was a difference in advice. I understand that SSL and SSH can be tied together and should be connected to a 100 K resister to GND.
As for using the TPS92613…
Could you tell me your application, we don't have a linear solution with 2A signal channel.
You can suggest your customer to use 3 pics of TPS92613-Q1 in this case.