Part Number: LP8865Y-Q1 Other Parts Discussed in Thread: TPS92620-Q1 Hi Sir,
When the EN pin is pulled low, is the fault pin also pulled low at the same time?
Could you please share the parameter for the delay time of fault?
Hi Vishnu,
Sorry for the late reply.
For output current-150mA devices with 2 channels devices, it is recommended to use two-channels devices TPS92620-Q1(up to 250mA) or TPS92622-Q1(up to 150mA).
Based on the function of thermal sharing, Thermal performance…
Part Number: TPS92622-Q1 Other Parts Discussed in Thread: TPS92620-Q1 , , TPS92623-Q1 , TPS92633-Q1 , TPS92624-Q1 Hi Team
Would like to ask about the specification of High Side Driver. Currently the customer is using the following two ICs, TPS2H160BQPWPRQ1…
Other Parts Discussed in Thread: TPS92602-Q1 , TPS92620-Q1 I would like to confirm the dimming ratio of TPS92602-Q1.
How much is the ratio of TPS92620-Q1?
The customer need 330mA * 2ch and the dimming ratio 10000:1 (must 5000:1).
If TPS92602Q1 can not realize…