Part Number: TPS92624-Q1 Tool/software: Dear Ti Team,
We are using below LED Driver.
input : 10V to 18V, output 5Volt LED.
output 200mA /per channel current 50mA
output 400mA /per channel current 100mA
output 600mA /per channel current 150mA
R1, R2, R3…
Part Number: TPS92624-Q1 Tool/software: Hi Team,
Can the TPS92624-Q1 not connect this resistor? Now the customer's heat problem is not serious, but the layout is not enough, so they want to remove the resistance.
Regards,
Ivy
Part Number: TPS92624-Q1 Tool/software: Hello,
Question 1)
I will supply the Supply pin of the TPS92624-Q1 IC with 5V, I want to use 3 channels in the circuit to drive 9.4mA LEDs (1 LED connected to each output Vled:2.1V) I want to use the remaining 1…
Part Number: TPS92624-Q1 Tool/software: Hello Ti Team,
This is Sanjay working in Vitesco technologies Bangalore, I need a P spice model for this chip, can you please share if available, I didn't find in the TI website
It would be great if you send…
Part Number: TPS92624-Q1 Tool/software: Hi Team,
May I know what is the TPS92623/24-Q1 quiescent current when the PWM pin is connected to GND? Thanks.
Regards,
Ivy
Part Number: TPS92624-Q1 Dear TI team,
I am trying to find the SPICE model from this part TPS92624-Q1 to run some simulations, however, I noticed there is no object. So could you please help me to obtain the SPICE model?
Best wishes
Arnulfo HH
Part Number: TPS92624-Q1 Hi,
The customer cannot update the schematic to the E2E due to security concerns.
I'd like to forward the schematic to you by email.
Please send me an email.
Mail : sr.cho@arrow.com
Part Number: TPS92624-Q1 Hi,
Please answer our customer's questions.
1. Whether PWMx is processed when OUTPUT DIMMING (PWM) is not used
- Do I have to use it above PWMx threshold voltage? Can I connect to Floating or GND?
2. Integrated output 4CH…
Part Number: TPS92624-Q1 Hi,
Please answer our customer's questions.
1. Whether PWMx is processed when OUTPUT DIMMING (PWM) is not used
- Do I have to use it above PWMx threshold voltage? Can I connect to Floating or GND?
2. Integrated output 4CH…