Part Number: TPS92630-Q1 Dears,
Pls kindly help to check the schematic as My design doesn't agree with the specifications,thanks.
T13J固定侧尾灯20240326(修改版).pdf
Part Number: TPS92630-Q1 We have received TPS92630QPWPRQ1 bought with different date code parts, upon comparison with X-Ray results, found that the leadframe of DC2224, DC2225, DC2226 differs with DC2414, 2415 as shown below:
Is there any PCN change on…
Part Number: TPS92630-Q1 Hi There,
My customer is using TPS92630 for Rev and Fog function in a rear lamp design. For the schematic, they have followed the application diagram in the datasheet, but they are stuck with some of the resistor calculations…
Part Number: TPS92630-Q1
Hi team,
This is FAE Jimmy support automotive application.
I have a question that since MCU is end-customer and my client is charge of designing LED part. the situation is that they would like to use MUC's GPIO to control LED…
Part Number: TPS92630-Q1 Hi team,
Do we have any data about the TEMP pin to GND resistance? Customer wants this to calculate the resistor.
Regards,
Peter
Part Number: TPS92630-Q1 when i use the TPS92630 IC, three channel apply ,refer to the following circuit:
PWM signal generated by MCU, IC driven three way LED, But when I disconnected one channel LED, the remaining two channel LEDs began to flash,
Why…
Part Number: TPS92630-Q1 hello, i have one question about the TPS92630 ic, i would like to achieve the LED dimming in/out , i think i need to apply the PWM control , I will adjust the PWM duty cycle from 0 to 100% to achieve LED breathing effect,Different…
Part Number: TPS92630-Q1 i have one question about the TPS92630 VIN PIN , I would like to know ,when the VIN VOLTAGE is 3V to 4V and EN connect to the VIN , Can the chip work properly and will an error be reported?
Part Number: TPS92630-Q1 Other Parts Discussed in Thread: TPS92633-Q1 , TPS92623-Q1 When customers use the design of TPS92630-Q1 as CHMSL, they find: When the initial power-on voltage of VIN is greater than 9V, gradually reduce VIN to 6.2V, the two light…
Part Number: TPS92630-Q1 Other Parts Discussed in Thread: TPS92633-Q1 Hello team,
Can you please confirm if below option is also applicable for TPS92630-Q1
In TPS92633-Q1 this is the option:
Request your input!
Thanks,
Madhura