Part Number: TPS92633-Q1 Hi team,
Customer want to use TPS92633-Q1. In design, each PCB requires a 2pcs chip, for the ICTR pins, can I connect the two chip pins together to share the thermal derating circuit? There are no corresponding application examples…
Part Number: TPS92633 Hi all,
My customer has their power supply on the anode, and wants to drive these LEDs from the cathode side. Can you advise in how this can be done via programming? It looks like it can be done, from this thread-
Their LED configuration…
Part Number: TPS92633-Q1 Hi team,
Please help to answer several questions:
1. What is the FAULT voltage if FAULT pin is floating, VSUPPLY>V(POR_rising), VEN>VIH(EN)
2. What is the FAULT voltage if FAULT pin is floating, VSUPPLY<V(POR_rising), VEN…
Part Number: TPS92633-Q1 Hi Team
i am using the IC (TPS92633-Q1) in simetrix simulation,when i try to Run the schematic it shows the error as shown in the below screenshot
Error:Encryption scheme not supported in this version
i cannot understand this…
Part Number: TPS92633-Q1 Hi expert,
I would like to double-check that
(1) Is TPS92633-Q1 a functional safety-quality managed product instead of a functional safety compliant product ?
(2) If it's a functional safety quality-managed product, does it…
Part Number: TPS92633-Q1 Hi Team,
If I have 2x92633s in my system would there be concern if I paralleled all 6 of the outputs to give me a single 900mA output?
Let me know your thoughts. Thanks for the help!
Best,
David
Part Number: TPS92633-Q1 Hi team,
My customer use 12V battery-DCDC 5V-92663 connection, due to some requirement, they need to detect short to 12V battery detection. I want to double confirm it is no problem.
Thanks!
Part Number: TPS92633-Q1 Hi
Datasheet said the output current is 150mA / channels.
But my customer test it and see it can output up to 350mA / channels
May i know the test condititon for this 150mA limitation ?
Part Number: TPS92633-Q1 Hi team,
If OUT3 is not used, it is no problem to left IN3, RES3 and OUT3 open and just connect PWM3 to ground, right?
If we don't use single LED short-circuit detection, how to connect SLS_REF? Thanks