Part Number: TPS92633-Q1 Hi team ;
I need TPS92633-Q1 IC's thermal derating table which has the power derating (W) due to ambient temperature (°C) for use in the thermal simulation.I kindly ask that can you provide it to me ?
Regards
Kara
'' TPS92633…
Part Number: TPS92633-Q1 Hello experts
Psipce simulaiton file given in the product page is seems to be not working. any other working simulation files ?
Regards
Part Number: TPS92633-Q1 Other Parts Discussed in Thread: TPS92633 , hello,
I have one question about the TPS92633 IREF PIN,I checked the DATASHEET and found that
The TPS92633-Q1 device has IREF pin to generate a high accuracy and low temperature shift…
Part Number: TPS92633-Q1 Our customer is evaluating TPS92633-Q1.
Input PWM signal from MCU to 7,8,9 pin of LED driver,The RGB_LED is lit with a constant current of 10mA for each of the three terminals.
The problem is that it lights up white and turns…
Part Number: TPS92633-Q1 Hi team,
Customer want to use TPS92633-Q1. In design, each PCB requires a 2pcs chip, for the ICTR pins, can I connect the two chip pins together to share the thermal derating circuit? There are no corresponding application examples…
Part Number: TPS92633-Q1 Hi team,
Please help to answer several questions:
1. What is the FAULT voltage if FAULT pin is floating, VSUPPLY>V(POR_rising), VEN>VIH(EN)
2. What is the FAULT voltage if FAULT pin is floating, VSUPPLY<V(POR_rising), VEN…
Part Number: TPS92633-Q1 Hi Team
i am using the IC (TPS92633-Q1) in simetrix simulation,when i try to Run the schematic it shows the error as shown in the below screenshot
Error:Encryption scheme not supported in this version
i cannot understand this…
Part Number: TPS92633-Q1 Hi expert,
I would like to double-check that
(1) Is TPS92633-Q1 a functional safety-quality managed product instead of a functional safety compliant product ?
(2) If it's a functional safety quality-managed product, does it…