Part Number: TPS92641
Hi,
Please review the following issue with our TPS92641 constant-current circuit.
Test conditions:
Input voltage: 48 V Target output current: 6 A Load: Resistive load Load resistance: Approximately…
Part Number: TPS92641 Hi team,
Customer is evaluating TPS92641, utilizing the UDIM pin to control ON/OFF state via High/Low signals from a MCU.
Similar to the issue described in the original thread, they have observed that the voltage at the RON pin…
Part Number: TPS92641
Hello,
I am designing an LED driver using the TPS92641.
The specifications are:
Vin = 49 V
Imax = 2.1 A
LED voltage = 12–48 V
Analog dimming down to 0%
The design is working; however, I noticed…
Part Number: TPS92641 Hi,
This is a follow-up question regarding the issue discussed in the following thread:
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1678599/tps92641-inquiry-regarding-output…
Part Number: TPS92641 Tool/software: Hello guys,
One of my customers is evaluating TPS92641 for their next products.
At this moment, they have the following questions. Could you give me your reply for them?
Q1. Is TPS92641 error amp (EA) output…
Part Number: TPS92641
Tool/software:
Dear Sir,
which is lower then 3.05V,(an internal reference), it can't work!
So can you give me some suggestion or other choice?
Part Number: TPS92641 Dear Team,
My cosutomer is designing the applicaiton circuit of the TPS92641. They consider to use the External Shunt FET PWM Dimming feature, and consider the layout of QSDIM and Cout. They think to set the Cout as 20uF + 0.1uF…
Part Number: TPS92641 Tool/software: Hi, I am using your TPS92641 to drive a laser. When I use the SDIM pin to dimming the light with PWM, there is an overshoot at the rise of the current waveform as shown in the figure below. I think this is caused by…
Part Number: TPS92641 Dear Team,
My customer is evaluating the TPS92641 application by modifying the TPS92641EVM. They increase V_IADJ from 0V to 2V (for V_CS=0.2V, ILED=5A). When ILED exceeds around 1A, on time becomes random or oscillalting. After…