Part Number: TPS92641 Tool/software: Hello guys,
One of my customers is evaluating TPS92641 using the device EVM for their new products.
At this moment, they have the following question. Could you please give me your reply?
Q. SW pin negative side…
Part Number: TPS92641 Tool/software: Hello guys,
One of my customers is considering using TPS92641 for their new products.
At this moment, they have the following question. Could you please give me your reply?
Q. TPS92641 datasheet says one of features…
Part Number: TPS92641 Tool/software: Hello guys.
One of my customers is evaluating TPS92641 for their next products.
[Their condition] Vin = 60V, Vout (Total LED Vf) =20V case and 50V case. Same TPS92641 board drives 20V LED or 50V LED. Iout = 10mA…
Part Number: TPS92641 Hello, my schematic diagram is shown below. The load is connected to a 14A/56V laser module, and the SDIM input is a 10Hz/10% duty cycle PWM wave. Currently, IADJ uses a regulated DC power supply to directly input 0.7V. Theoretically…
Part Number: TPS92641 Other Parts Discussed in Thread: LM3409HV , , , LM3409 Tool/software: Dear respected TI experts,
I have implemented a LED driver with shunt dimming feature by using LM3409HV. It works well with high dimming performance.
Now…
Part Number: TPS922055 Other Parts Discussed in Thread: TPS92641 ,
Tool/software:
Hi,
How can I request the latest SIMPLIS models of the following two parts?
TPS922055 and TPS92641
Currently the TPS922055DMTREVM is out of stock, so we urgent…
Part Number: TPS92641 Other Parts Discussed in Thread: LMG2100R026 , Tool/software: HI team,
My customer interested in GaN for power stage for lighting.
Can TPS92641 use with TI half bridge GaN such as LMG2100R026?
Regards,
Hayashi
Part Number: TPS92641
Dear TI Team,
Request a schematic review of the TPS92641.
Input Voltage: DC48V
Output Voltage ( LED String Voltage - VLED) : DC45V
LED Vf: 3.2V
LED Current (ILED) : 7A