Part Number: TPS92660 Other Parts Discussed in Thread: TPS92390 Tool/software: Hi
Could you help confirm whether TI has recommended products
LED driver IC specification requirements are as follows, thank you
S pec: Voltage 85V~102.3V; Current 0…
Part Number: TPS92660 Other Parts Discussed in Thread: TPS92561 Tool/software: Hello There,
I have an application where I’ll need to power different UV LED strings. Below are the specification requirements. Could you help me with suggestions for LED…
Part Number: TPS92660 Other Parts Discussed in Thread: TPS92640 , Hi,
I have been using TPS92640 in my existing design. Unfortunately the part is out of stock. I am thinking of moving to TSP92660, need suggesstions on design. Do I need an external buck…
Part Number: TPS92660 Hi,
Need design review of the below design:
Need to know if the FET selected is K, considering the PWM switching frequency is around 200 - 300 KHz. Also, is the inductor selected is good. Input voltage typical is going to be…
Part Number: TPS92660 helleo , I need to drive a laser diode array, total 8 strings , each string voltage about 35V, constant current 2.5A(typical), 3A(max), TPS92660 can be current trimmed by I2C interface, and achieve PWM current, it is good for me…
Part Number: TPS92660 As for the use of ladj, the PWM signal needs to be filtered by RC and shaped into a triangular wave input as shown in the figure below, right? Instead of directly inputting PWM signal.
Other Parts Discussed in Thread: TPS92660 hI, I would like to Know whether is it possible to control the two strings of LED separately in IC TPS92660.(i.e.When one sting of LED is ON, THe other one must be in OFF condition & vice versa)
Binod,
Here are some products I think are similar that could work for you. I'll email the product lines who own these parts internally with a link to this thread so they can provide further comments.
UCC28C43-EP
TPS92410
TPS92660
LM3401
TPS92630…
Hello,
What do you mean by 7-segment LED, 7 LED strings or 7 LEDs?
We do have some DC/DC drivers that support I2C function like LM3463 and TPS92660.
You can take a look on TI’s website.
Thanks.