Part Number: TPS92662-Q1
We are interfacing the led driver with SAM controller and sending a UART packet {0x87,0xBF,0x80,0x36,0xB8,0xE4} for configuring SYSCFG register and there after reading SYSCFG register with command {0x4B,0xBF,0x80,0x01,0x86}…
Part Number: TPS92662-Q1
Hi,
Hope you can help us we are using the TPS TPS92662-Q1 (8 MHz) with a can transceiver TLE9251SJXUMA1 as the diagram below, and we just want to turn ON one led to start development other things but we cant perform the function…
Part Number: TPS92662-Q1 Dear Sir,
I have some issue on setting the LED driver to output maximum.
I'm setting channel 1 to 999 but when I check the waveform there are still a PWM pulse. Is this normal? or what is the correct setting to output…
Part Number: TPS92662-Q1 Want to know the difference between 92662 and 92661?
And output current needs 1A, I don't know if 92661 can be used up to 100% Would that 92626 be better?
How to get technical documents and detailed specifications about TPS92662…
Part Number: TPS92662-Q1 Dear Sir/Ms.
I would like to ask if the TPS92662 can be connected as shown below, through the DEVID segment in the communication protocol. DEV_ID[4:0]. Set as follows: RH: TPS92662 : DEV_ID[4:0]0x01 MCU: DEV_ID[4:0]0x03
…
Part Number: TPS92662-Q1 Hello,
I want to know below questions about TPS92662-Q1. Please help! Thanks!
1. Is it grounded when not using pin 15 ADC2 or pin 17 ADC1?
2. Is there a special requirement for the selection of 8Mhz crystal oscillator? Can…
Part Number: TPS92662-Q1 Regarding soldering QFP-48 package of the TPS92662-Q1
In the Datasheet there is a lead to Package height tolerance given of 50-150µm. Since the package has thermal pad, this tolerance has impact on solder print volume requirements…
Other Parts Discussed in Thread: TPS92662-Q1 We have question about TPS92662-Q1.
We checked the datasheet of TPS92662-Q1.
We need more information about using this IC.
Question 1.
We want to know pin number of each pin name.
For example…
Part Number: TPS92662-Q1 Please share sample codes to interface with TPS92662QPHPRQ1 via UART. Also do share the sample code for interfacing an I2C EEPROM with the device.