Part Number: TPS92682-Q1 Tool/software: Hi team,
My customer is evaluating TPS92682-Q1 in their project and met below issue, could you help give some comments?
In CC mode, CHxVU is set to 1 in the FLT register when the output is shorted to ground…
Part Number: TPS92682-Q1 Tool/software: Hello, expert.
The SPI waveform of TPS92682 is also measured. The waveform of TPS92520 is found to be different. The rising and falling time is relatively long. Our configuration is as follows: 1 TPS92682 +3 tps92520…
Part Number: TPS92682-Q1 Tool/software: Hello, expert,
we are currently using the scheme of TPS92682 * 1 + TPS92520 * 3, two-phase Boost +6-phase Buck constant current;
The boost voltage is 51V; PWM frequency of TPS92520: the 215hz
Load configuration…
Part Number: TPS92682-Q1 Tool/software: Hi team
what is the minimum storage temperature? i see most of automotive product the minimum storage temperature is -65 degree C.
Part Number: TPS92682-Q1 Tool/software: Dear TIer,
According to Figure 7.3, the synthesized signal (SLOP & iSW) cannot trigger VCOMP. How can GATEx determine whether it is on or off?
Part Number: TPS92682-Q1 Tool/software: Hello, expert,
We need to know this parameter to do a register initialization operation, thank you.
We want to know that the input voltage of TPS92682/TPS92520 decreases, and the register contents of TPS92682…
Part Number: TPS92682-Q1 When OVOPT is set to 1, an overvoltage fault occurred, and the closing of Gate 2 was 5ms later than that of Gate 1. When OVOPT is set to 0, an overvoltage fault occurred, and both Gate 2 and Gate 1 closed simultaneously. I would…
Part Number: TPS92682-Q1 Hi team,
Can you help review our schematics attached below ?
We have a TPS92682 design with the following design conditions
Vin = 9~16Vdc
CC mode
Iout = 0~4A with 5 ohm load
Currently, it can output 2A normally, but…
Hi Venkatesh,
Venkatesh K J said: Internal vs. External PWM for FET Control :
- Being that this is a simulation, there will be no difference in using external versus internal PWM source. Therefore, I attached a pulse to the PWM pins at the desired…
Part Number: TPS92682-Q1 Other Parts Discussed in Thread: TPS92691-Q1 , TPS92691 Tool/software: Hello,
We have made a design that runs a 37V@1A forward voltage LED with a 48V power supply nominal, max 52V.
I've followed the design guide for TPS92691…