Part Number: TPS92682-Q1 Tool/software: Dear TIer,
According to Figure 7.3, the synthesized signal (SLOP & iSW) cannot trigger VCOMP. How can GATEx determine whether it is on or off?
Part Number: TPS92682-Q1 Tool/software: Hello, expert,
We need to know this parameter to do a register initialization operation, thank you.
We want to know that the input voltage of TPS92682/TPS92520 decreases, and the register contents of TPS92682…
Part Number: TPS92682-Q1 Tool/software: Hi team
what is the minimum storage temperature? i see most of automotive product the minimum storage temperature is -65 degree C.
Part Number: TPS92682-Q1 When OVOPT is set to 1, an overvoltage fault occurred, and the closing of Gate 2 was 5ms later than that of Gate 1. When OVOPT is set to 0, an overvoltage fault occurred, and both Gate 2 and Gate 1 closed simultaneously. I would…
Hi Venkatesh,
Venkatesh K J said: Internal vs. External PWM for FET Control :
- Being that this is a simulation, there will be no difference in using external versus internal PWM source. Therefore, I attached a pulse to the PWM pins at the desired…
Part Number: TPS92682-Q1 Tool/software: hello expert
When TPS92682 uses CV mode, what is the difference between selecting internal PWM and external PWM? If internal PWM is selected in constant voltage mode, will it affect the output?
Part Number: TPS92682-Q1 Other Parts Discussed in Thread: TPS92691-Q1 , TPS92691 Tool/software: Hello,
We have made a design that runs a 37V@1A forward voltage LED with a 48V power supply nominal, max 52V.
I've followed the design guide for TPS92691…
Part Number: TPS92682-Q1 Hi team,
Can you help review our schematics attached below ?
We have a TPS92682 design with the following design conditions
Vin = 9~16Vdc
CC mode
Iout = 0~4A with 5 ohm load
Currently, it can output 2A normally, but…
Part Number: TPS92682-Q1 Tool/software: hello,
About the UV FAULT,The datasheet have the following descriptions,i would like to ask
if i set the 2PH=1,CH2UV fault is disabled, I apply the Two-phase mode
I would like to ask what is the value of CH2UV…