Part Number: TPS92682-Q1 Other Parts Discussed in Thread: TPS92518 Hi TI support teams,
Our project is working with the TPS92682-Q1
Simple diagram can be shown like below:
I want to ask that do TI have any sample Linux driver to control the TPS92682-Q1…
Part Number: TPS92682-Q1 Hi,
The register 0x25 is only for two phase application, it should not be
accessed in two channel application, right?
BTW, two phase application is only supported in CV setting, not in
CC setting, right?
Honda
Part Number: TPS92682-Q1 Hi team,
I saw in datasheet, the FB2 pin is floating in CV mode two-phase BOOST configuration. Is there any special consideration? Can we connect it to GND?
Thanks.
Part Number: TPS92682-Q1 Hi, Team
Hope you are doing well!
My customer want to use our TPS92682-Q1 in CC mode to supply position light.
The minimum output current required is 6mA.
The input voltage range is 9~16V, the output voltage required is 45~50V…
Part Number: TPS92682-Q1 Hi team,
My customer want to use TPS92682 in two conditions as below, could you please help to evaluate the application possibility and limitation?
1. Configurate the 2 channels as: Buck-Boost CC mode. Vin=7~18V, Vout=50V, Iout…
Part Number: TPS92682-Q1 Hi team,
Can tps92682 turns on channels without MCU configuration after power up?
Customer has a requirement: assume MCU is fault after power up, they want the output channels are on.
Thanks!
Part Number: TPS92682-Q1 Hi team,
My customer want to achieve that 2*TPS92682 along with 1*MCU, could you kindly tell me how to save MCU IO resource?
For example, 1*TPS92682 typically need 2*FAULT, 1*SPI. Can 2*TPS92682 use 1*SPI? Thanks!
BR
Jiawei
Part Number: TPS92682-Q1 Hi expert!
Here's a question that if the device lose power, after the power recovers will the values in LH registers maintain as configured before or be erased as default values 00000000?
Many thanks!
Part Number: TPS92682-Q1 team,
I was hoping the SW available on ti.com EVM-069 would contain it but it doesnt : can you please point me to the C code ( or CCS project ) containing the SPI driver and exmple code to generate working SPI frame for the 682…