Part Number: TPS92691-Q1 Tool/software: Hello,
I am planning to use TPS92691-Q1 for a LED driver design and I intend to use it in BOOST mode. In my design I don't intend to use the PWM dimming functionality, so if I tie PWM pin to VCC, would I still…
Part Number: TPS92691-Q1 Tool/software: I have a problem where the gate pin is activated as soon as only the Vin pin is supplied with 13V. Has anyone had a similar problem?
Thanks
Part Number: TPS92691-Q1 Other Parts Discussed in Thread: TPS922052 , LP8868Z-Q1 Tool/software: Hi Teams,
The customer is looking for a backlight driver solution, similar to BL9582B, that drives 2x3W infrared LEDs in series. When inputting 12V, the…
Part Number: TPS92691-Q1 Other Parts Discussed in Thread: TPS92692 , TPS92691 Hi team,
As the title, could you kindly tell me what is the difference between TPS92691 and TPS92692? Thanks!
BR
Jiawei
Part Number: TPS92691-Q1 Other Parts Discussed in Thread: TPS92691 I've been working on a design using this LED driver (albeit, we're using it with a laser diode) for a couple days. Please see the schematic below.
Without going into too many details…
Part Number: TPS92691-Q1 Hi team,
could you help tell me the Minimum duty cycle for boost of 92691 cause there is only the max duty cycle in DS, thanks
Part Number: TPS92691-Q1 Other Parts Discussed in Thread: TPS92691 We are investigating using the TPS92691 in a buck-boost topology. The power supply that we are using to power the LEDs is 48 V. We need between 36.4 V and 52 V out. I will note that we…
Part Number: TPS92691-Q1 I'm debugging a design for a project that we've already prototyped and tested. I know that the design works. Anyhow...
We soldered the first one on Friday. The only difference is that we didn't solder the DAC and buffer (which…
Part Number: TPS92691-Q1 Other Parts Discussed in Thread: TPS92691 Hi, Team
My customer is using our TPS92691 as Sepic CC mode.
The load is 6 LEDs, output constant current is 1A, and the load voltage is 3V/per LED.
Now customer engineer measures…
Part Number: TPS92691-Q1 Other Parts Discussed in Thread: TPS92691 I've designed a switching controller using this chip for use with a large LED array. It's still in a prototype stage, so I'm using a potentiometer/voltage divider to adjust the voltage…