Part Number: TPS92691EVM-001 Other Parts Discussed in Thread: TPS92691 I would like to purchase the EVM for the TPS92691 LED driver for initial validation but I would like to power it from 55V, as it will be the condition of the final project. Is is possible…
Part Number: TPS92691EVM-001 Hello guys,
One of my customers bought TPS92691EVM-001 to evaluate the device for their next products.
They want to modify this EVM for buck mode only because the conditions of their next product are VIN=24V, VOUT(LED…
Part Number: TPS92691EVM-001 Hi team,
Another question about TPS92691EVM-001
1.When using the recommend PWM input for dimming , I found the output current has a surge current on the rising edge of the PWM input voltage. The maximum of the overshoot…
Part Number: TPS92691EVM-001 I want to change Low side current sense on TPS92691EVM-001, please let me confirm about chip size of R24.
Datasheet is not described these information;
I looked like R24 is 1206 (inch) by assembly drawing, is it correct…
Part Number: TPS92691EVM-001 Hi
after reviewing the schematic I ASSUME I change R1 for higher current. However it is a single diode VF = 1.8V @ 1.5A. Most of your applications are or boost configuration for more than 1 LED. The evm datasheet does…
Issac-san
Thank you for reply,
The reason for choice TPS92691EVM-001 are two points below;
・Higher Vout condition need to change low-side current sensing from below E2E thread.
https://e2e.ti.com/support/power-management/f/196/p/867907/3242547…
Part Number: TPS92691EVM-001 Other Parts Discussed in Thread: TPS92691-Q1 Hello,
I'm currently looking for a LED driver with the following specs:
Input voltage : 48Vdc
Output voltage : 2 - 60Vdc
Current drive value: 100mA - 1500mA
PWM pin…