Part Number: TPS92692-Q1 Tool/software: During specific environmental tests, 60 units of TPS92692-Q1 were tested under constant damp heat conditions for a week, with a temperature of 55 degrees and a humidity of 80%. The lamps were operated at a voltage…
Part Number: TPS92692 Other Parts Discussed in Thread: LM3410 Tool/software: Dear Sir/Mam,
Can you share some Information for this IC " TPS92692 ".
What is the dimming frequency and output current for this IC, I have mentioned our requirement below…
Part Number: TPS92692-Q1 Hello experts, I'm having trouble passing the superimposed AC current test when testing the TPS92692. This test checks the DUT's immunity to ripple voltage in the vehicle system. The injection frequency range is 10Hz~30kHz, VIN…
Part Number: TPS92692 Tool/software: Hi team,
I'm planning to include a small control circuit with thermistor and FETs to pull-down the SS pin. Is it ok to power this control circuit from VREF (or VCC) of this IC?
The current required is around 5mA…
Part Number: TPS92692 Tool/software: Hi,
We would like to consult with you regarding high-power LED driver solutions using TI products.
Currently, we are using the ADI LT3966 under the following conditions:
Input voltage: 24V
Output voltage…
Part Number: TPS92692-Q1 Other Parts Discussed in Thread: TPS92692 Tool/software: Hi
Our customer has raised some questions about the TPS92692:
1, In the datasheet table2 gives the calculation formulas for G0, wp, wz, could you please tell me about…
Part Number: TPS92692 Tool/software: Hi TI,
I'm confused about below description of current limit threshold in TPS92692 datasheet. When PWM signal is low, the DCDC stops switching and there's no current sensed by IS pin, why the current limit threshold…
Part Number: TPS92692 Tool/software: Hi TI,
I'm designing a boost controller and a little confused about the slope compensation calculation of TPS92692. For boost topology, how to derive formula (31) in datasheet from formula (4)? Thanks.
Part Number: TPS92692-Q1 Tool/software: Hi,
I am working on sepic conerverter design for below spcification.
Vin 8V to 16V
Vout 21V
Iout 0.75A
Fsw: 400KHz
i am checking MOSFET drain waveform from 8V to 16V. Till 13V VDS signal is ok. when…
Part Number: TPS92692-Q1
Hi team,
I want to check the conflict between the description and calculation.
The description shows Ris, and the equation shows Rslp. What is the right one?
I am asking this question, because customer find when decreasing…