Part Number: TPS92692-Q1 Other Parts Discussed in Thread: TPS92692 Hi TI Team,
I'd like to ask you if PSPICE simulations of attached tests are possible. If possible, I will send my customer's schematic. Please check it and let me know.
TPS92692…
Part Number: TPS92692-Q1 Other Parts Discussed in Thread: TPS92691-Q1 , TPS92692 What are the main diferences between TPS92692-Q1 and TPS92691-Q1?
Thank you
Part Number: TPS92692-Q1 Other Parts Discussed in Thread: TPS92692 Hi, to whom it my concern.....
I intend to use TPS92692 for a Buck-Boost LED driver as suggested in the datasheet:
The application is a headlight for +12V and +24 vehicles. So the pecs…
Part Number: TPS92692-Q1 Hi,
I have a board designed to driver 9 LEDs with a forward voltage approx 20V, max current ~700mA, dimming avg ~35mA, sw freq 390 khz, RCS 0.240.
The circuit works well in high brightness mode down to 6V and passes stop start…
Part Number: TPS92691-Q1 Other Parts Discussed in Thread: TPS92692 , TPS92691 Hi team,
As the title, could you kindly tell me what is the difference between TPS92691 and TPS92692? Thanks!
BR
Jiawei
Part Number: TPS92692-Q1 Other Parts Discussed in Thread: TPS92692 Hi Expert,
Our customer has a new request. It's a DMS application and ASIL-B system level is required. The output voltage is about 12.8V (4 LEDs serial) and current is 3A. I see we only…
Part Number: TPS92690-Q1 Other Parts Discussed in Thread: TPS92692 , TPS92692-Q1 Tool/software: Hi Team,
Regarding the material in the title, can I get a file without protection as I would like to see the formulas for each item?
I don't understand why…
Part Number: TPS92692-Q1 Other Parts Discussed in Thread: TPS92692 Hi
I got a question from customer that is there any concern using TPS92692-Q1 as constant voltage ?
Any comment, thanks!
Part Number: TPS92692-Q1 Other Parts Discussed in Thread: TPS92692 Dear Sir/Ms.
My customer is looking for MTBF design parameters. Find the file below TI, the parameters inside are different from those on the webpage. My client designed TPS92602BQPWPRQ1…
Thank you For your Reply,
TPS92691-Q1 not available in Pspice, TPS92692-Q1 is available, here I have mentioned the requirement,
Major parameter is less Dimming Frequency 1Hz to 40 Hz, But TPS92692-Q1 mentioned as typ 240Hz.
Input Voltage: from 3V to ma…