Part Number: TPS929120-Q1 Hi Team, I am looking for a Automotive grade LED Driver with Lin interface and protection features like over and under voltage protection and reverse polarity protection. Does this support all the features if not please suggest…
Part Number: TPS929120-Q1 Tool/software: Dear Mr omkar ,
Our customer has detected recently a problem on the PN 1032947A NPF TPS929120QPWPRQ1 with DC 2411
Defect : Tail function is not working on rear lamp
Would you confirm us to return…
Part Number: TPS929120-Q1 Tool/software:
Hi,
Since both the TPS929120QPWPRQ1 and TPS929160QDCPRQ1 support the FlexWire control interface, are their firmware the same?
Thanks & best regard
Part Number: TPS929120-Q1 Following commands I am using for my BCM, now my requirement is for slave 0, and channel 0,1 , my bcm should detect a n-1 and open fault.
For n-1 fault, voltage should be less than 6 Volt
For open fault, voltage should…
Part Number: TPS929120-Q1 Tool/software: I am currently performing some functionality tests for the TPS929120-Q1 and I encountered some interesting behaviors.
As a test environment we use a power supply set to 12V and 3 output channels for the TPS929120…
Part Number: TPS929240-Q1 Other Parts Discussed in Thread: TPS929160-Q1 , TPS929120-Q1 , Tool/software: Hi team,
May I ask if the TPS929120-Q1, TPS929160-Q1 and TPS929240-Q1 are compatible in one system? Thanks.
Regards,
Ivy
Part Number: TPS929120-Q1 dear texas team ,
we have opened a case with the number CPR241098975 for the PN TPS929120QPWPRQ1 and we have submitted a request for the unit return for failure analysis , we have already send clear pictures to m-chowdhury…
Part Number: TPS929120-Q1
Do you have a recommended or specific protocol (method, procedure) for loading the software into the drivers?
If yes, can you share this method with us?
If for the drivers, at the tester level we were unable to carry…
Part Number: TPS929120-Q1 Tool/software: Dear support team,
can you please specify the leakage current of a channel when it is disabled (OFF) by CONF_ENCHx.
Best regards,
Andreas
Part Number: TPS929120-Q1 Tool/software: HI Team,
Hope all is well.
My customer is Xingyu.
Currently they want to use this device for platform design, so they hope to have a standard schematic design that can be used in different projects.
I understand…