Part Number: TPS929120-Q1 I have to program the eeprom of the device TPS929120-Q1.
I'm using the mode with Ref pin high, address 0x0
but when I write the register "conf_misc7" with the value 0x1 this register remains 0x0. If I try to write 0x2…
Part Number: TPS929120-Q1 Hello,
do you have additional information about EMC behaviour of the IC? Interesting would be for example results for DPI (Direct Power Injection).
Thank you.
Part Number: TPS929120-Q1 Other Parts Discussed in Thread: TPS929121-Q1 , Hi, Team
Hope you are doing well!
My customer has two questions about our TPS929121-Q1, please kindly help to explain.
1. Customer knows that the only difference between TPS929120…
Part Number: TPS929120-Q1 Hi
now I do some test with our discrete components, I want to test the performance under high UART data rate, could you please tell me how to change the date rate through your GUI, thanks !
Part Number: TPS929120-Q1 Hello,
what should we do with the unused outputs, if we only use 6 of the 12 outputs? Should they be left open or pulled to GND or Supply? In the configuration they are not enabled.
Thank you
Part Number: TPS929120-Q1 Hi Ben,
Can 929120 detect short to battery fault? Are we able to use the LED open-circuit fault detection which is VSUPPLY-VOUT<VOPEN_TH_RISING? If we can, how to distinguish open fault from short to bat fault?
Thanks!
Part Number: TPS929120-Q1 I have downloaded S9KEAZ128 Demo Codes.zip and read it . there are some question about it.
As below, in function UartWrite(), UART2_C2 |= UART_C2_RIE_MASK was commented. i think it will lead to UART2_IRQHandler() don't working.…
Part Number: TPS929120-Q1 Hello,
Can we have communication between MCU and TPS929120-Q1 directly without any CAN transceivers?
What are the concerns arising out of long distance communication? How to ensure signal integrity if design has 3 boards and…