Part Number: TPSF12C1 I am designing a DC to DC Power supply for telecom application in I would like to know if a psophometric filter can be implimented using TPSF12C1 at the ouput of the DC to DC converter. Output power is 600 W.
Thanks
-Mani
Part Number: TPSF12C1-Q1 Hi team,
We found FIT rate difference between "FuSa information" and "Quality, reliability & packaging data download". Could you tell me why each FIT rate is different? Which one could we use?
"FuSa document…
Part Number: TPSF12C1-Q1 Please confirm that the order of the leads in the red circle of TPSF12C1-Q1 can be changed at will? For example, 1A and 1B were originally connected to the L line, but now they are connected to the N line. If it can be swapped…
Hi again,
Am I doing something wrong, or does this AC model only work for injecting a signal on the "STAB" pin, as how the provided PSpice schematic is configured? I would like to be able to place a common-mode AC signal anywhere (for example…
Part Number: TPSF12C1 Other Parts Discussed in Thread: LM25149 Can this part be used on a 28 VDC bus. The noise source is an isolated 150 W DC-DC converter (Forward).
Thanks
Other Parts Discussed in Thread: TPSF12C1
Dear TI Support Team,
I hope this message finds you well. I am reaching out regarding the active evaluation module based on the TPSF12C1. During my testing and evaluations, I've observed that the module…
Part Number: TPSF12C1 Hi team,
My customer is considering using TPSF12C1 in their next-gen robot design.
Could you please advice on the following concerns of the customer?
1. Robot noise frequency varies from 4kHz - a few MHz . Is there a way to deal…
Part Number: TPSF12C1-Q1 Is it possible to use the TPSF12C1-Q1 for single Phase 1000V DC Applications?
The system in question is a DC/AC inverter and would benefit from the active CM noise rejection.
Part Number: TPSF12C1 Hi Team,
can you help with the following customer question:
I have a question regarding the TPSF12C1 chip. The drives we develop have a voltage between 24V-60V (48V nominal). We are considering using this chip to filter the common…
Part Number: TPSF12C1 Hi TI Team,
We at Larsen and Technology Services found this IC very interesting.
Our objective is to suppress the leakage current generated by common mode (CM) voltage particularly at 4 kHz switching frequency. Can this work in…