Part Number: TPSI3050-Q1 Other Parts Discussed in Thread: AMC1311 , TPSI3050 Hello,
We are working on a board with a 400V power input. We have an isolated 5V section to power our MCU and a few other LV Circuits. We need to monitor the voltage of our supply…
Part Number: TPSI3050-Q1 Other Parts Discussed in Thread: AMC1311 , TPSI3050 , Hello,
We are working on a board with a 400V power input. We have an isolated 5V section to power our MCU and a few other LV Circuits. We need to monitor the voltage of our supply…
Part Number: TPSI3050 Hi, when will this product have the formal certiifcation to IEC 60747-17 (VDE 0884-17)? It looks great but I cannot design it into our product until it has the certification. Thanks, James
Part Number: TPSI3050-Q1 Hi,
The customer is conducting EMC testing of the precharge relay.
2630.Schematic.pdf EMC Test 2 Condition
- During operation, enter the waveform randomly into the J1 connector.
Input Point : J1 con 1 pin : + COM, J1 con 13 pin…
Part Number: TPSI3050 Hi Team,
in the two-wire mode of the TPSI3050, is the enable/disable possible by connecting/disconnecting the VSSP pin and related node components to/from the primary side ground?
For example, with reference to the figures:
1) the…
Part Number: TPSI3050-Q1 Hi,
The customer is using TPSI3050-Q1 for Precharge relay.
1. EMC Test (BCI) Condition
- Measure the Gate Driver (TPSI3050-Q1) output signal after applying DC +12V in the Precharge stage
- Precharge resistance, relay resistance…
Hello Tejasri,
TI does not support simulation in LTSpice. These models have been created for and verified with PSpice for TI:
https://www.ti.com/tool/PSPICE-FOR-TI
Best regards, Tilden Chen
Solid State Relays | Applications Engineer
Part Number: TPSI3050 Hello,
I have not found any application or example circuit where the VDDH is used to supply the auxiliary circuit of the isolated side, so I wonder if this could be possible.
Thank you and regards.
Part Number: TPSI3050 Hi Team,
could you check if we can replace HT0740LG-G with TPSI3050.
Here is our current schematic with HT0740LG-G
Best Regards,
D.