Part Number: TPSI3052 Can you review this an make sure im on the right track? D of Q1/Q2 are a high side switch where Q1 D is 400VDC. EN is a 5V signal Q1 has a total gate charge of 75nC. Should I add a gate resistor and a shottkey diode on the VDRV line…
Part Number: TPSI3052 I am looking into selecting a TPSI3052SQDWZRQ1 as a high side precharge. Im looking at the applications schematic and see two NMOS being used for reverse power protection, but it is unclear if it is high side or low side. If it is…
Part Number: TPSI3052-Q1 Hello, I would like to use TPSI3052QDWZRQ1 in a non Isolated Application, so in the system VSSP and VSSS would be the same. The reason I want to use this is becsue I want a 15V gate drive from a 5V supply. Is this acceptable …
Part Number: TPSI3052 Tool/software: Hi TI Support Team,
I am using the part TPSI3052 Gate Driver IC in my Current Design may I know what is the minimum and absolute Enable Current that is required for the gate driver IC (TPSI3052) when it is working…
Part Number: TPSI3052 Hello, Experts
I'm considering using the TPSI3052 as reinforced insulation. Due to application requirements, compliance with IEC 62368-1 is necessary, and Section 5.4.4 of this standard specifies requirements for solid insulation…
Part Number: TPSI3052-Q1 Other Parts Discussed in Thread: TPSI3100 Hi team,
I am planning to use TPSI3052-Q1 to driver contactor(high side relay).
Then I have a quesion about the supply current of this device.
IVDDP is specifed 37mA typican when…
Part Number: TPSI3052 Tool/software: Hello,
I have a question about the behavior of the VDDP supply in the TPSI3052. Would it be possible to switch the VDDP off for short periods, while keeping the Enable pin high and still get VDRV high on the secondary…
Part Number: TPSI3052 Other Parts Discussed in Thread: TIDA-050058 , TPSI3100 I have an application where I need to switch a boiler of max 3kw every 10 seconds. Hence I want to implement the following SSR circuit:
Can handle 230VAC
Max 13A continuous…
Part Number: TPSI3052-Q1 Other Parts Discussed in Thread: TIDA-050063 , TPSI31PXQ1EVM Tool/software: Hello TI team
I'm Zhuo Li, an electrical engineer from Sunwoda Mobility Technology Co., LTd(Tier1 battery system supplier).
Our department is very…
Part Number: TPSI3052-Q1 Other Parts Discussed in Thread: TPSI3052 Tool/software: Hi,
I'm using the TPSI3052-Q1 in my design in two instances:
1. as a driver to a high side SiC MOSFET in a similar application as the colleague complaining about the…