Part Number: TPSI3052-Q1
Tool/software:
Hello,
Is it possible to get the weight/mass (mg) information for following item:
TPSI3052QDWZRQ1
Thanks & regards,
Pawel
Part Number: TPSI3052
hello,
I'm considering using this Isolated switch driver for our new designs. can you provide me more information, regarding the diffrence in perfomence for driving VDDP 3.3 volt supply VS driving VDDP 5 volt supply.
Part Number: TPSI3052-Q1
Tool/software:
Hi team,
Is there any working Spice model of SSR IC with 15V, from the ti website it is not working spice showing the simulation error.
Can ti help us to solve this issue?
Regards
Vivek
Part Number: TPSI3052-Q1
Tool/software:
Hi,
I am using the simetrix model of TPSI3052 in my simulation which i got from "e2e.ti.com/.../tpsi3052-q1-request-for-simetrix-model"
I did notice that when simulating this model at high temperature the output node 'DRV' declines to 0V, even when Enable line is pulled up throughout.
I need some help in understanding what this model behavior. Is this intended or just a model issue?
Part Number: TPSI3052-Q1
Tool/software:
Customer would like to get the certificate report for UL1577 & IEC60747. Could you help to support it!
Regards
Brian
Part Number: TPSI3052-Q1
I download the simulation model from TI official website but it didn't work when i did the circuit simulation with LTSpice. the error as below:
Pls help to check if the model has some probelm and how to solve it.
Fatal Error: Undefined subcircuit: and2
Part Number: TPSI3052
Tool/software:
Hi team,
Customer input value to understand tstart value is arroung 2[ms]: TPSI305x_calculator_1p24.xlsx
The definition of tstart is the time to VDRV = HIGH from EN=HIGH.

But customer also understands VDDH and VDDM is supplied from VDDP without EN = HIGH. so the charging time to C_DIV should be tstart.
In other words, if C_DIV is charged enough, the time to VDRV= HIGH from EN=HIGH must be t_LH_VDRV (185 us typ) in the datasheet.
Is customer understanding correct? because customer doesn't accept 2ms, require shorter.
So the question is that if Cdiv1 and Cdiv2 charged well after tstart from VDDP supplied, the delay of VDRV and EN must be t_LH_VDRV, is that correct?
Best regards,
Hayashi
Part Number: TPSI3052-Q1
Tool/software:
Can you supply a spice model for TINA?
B.R
Shaya
Part Number: TPSI3052-Q1
Tool/software:
Hi Team,


1. I'm looking for an active high-side precharge MOSFET driver for a 300V system with an AC input voltage range of 90VAC to 180VAC, followed by a diode bridge rectifier. I found that this driver is suitable for my application,
2. But in the simulation, the gate drive signal is not following the enable input command. Could you please help me resolve this issue
Part Number: TPSI3052
Hi tI team,
Can TPSI3052 do the driving NMOS to do the switch on the high side?