Part Number: TPSM33615 Tool/software: Hello team -
On my CCA, I have the TPSM33615 “F” version installed to convert 28V to 5V. I have the MODE/SYNC pin 11 connected to VCC to generate Fs=1MHz because I thought I was using the RT version (“non-F” version…
Part Number: TPSM33615 Other Parts Discussed in Thread: TPSM63602 Tool/software: Hello team,
Can TPSM33615 be used at the below condition? According to the datasheet, Vout (TPSM33615 can output) is up to 14V.
Vin: 18V~30V (24V typ) -> Vout: 15V, 1A…
Part Number: TPSM33615 Tool/software: Hi team - Can the TPSM33615 be used as an inverting buck like shown in the TPSM5601R5HRDAR datasheet?
Thanks,
Jacob
Part Number: TPSM33615 Tool/software: Hello, our PCBA manufacturer has sourcing problems for TPSM33615RDNR (and also TPSM33625RDNR). I received the question, if they can use TPSM33615FRDNR as this part is available. In our system, there are use cases…
Part Number: TPSM33615 Other Parts Discussed in Thread: LM66200
Tool/software:
Hello,
I am working on an application with the TPSM33615 and I am seeing behavior where VCC remains under 3V (only rises to ~1.9V). My schematic is configured for a 5V…
Part Number: TPSM33615 Tool/software: Team,
My customer plans to use our TPSM33615FRDNR in their design.
They need to externally synchronize it, and, sync signal will start after device itself.
They have reviewed the DS (especially p. 18) but need…
Part Number: TPSM33615
Tool/software:
I am building a design with the TPSM33615RDNR. I have 18Vin and 12Vout @ 1A max. The datasheet just seems to give a table to pick the switching frequency, but doesnt seem to provide any equations to check other…
Part Number: TPSM33615 Hi,
My question relates TPSM33615 DCDC module:
My application requires buck DCDC converter to 12VDC out from 24V automotive input which may vary between 18 to 32V but sometimes it may go downto 8V for short period of times…
Part Number: TPSM33615 Other Parts Discussed in Thread: LMR60410 Tool/software: Hi,
I am looking for a power step-down solution for:
Input Voltage can be either fixed 5V or range from 8-18V.
Output current 1A
Output voltage range from 0.1…
Part Number: TPSM33615 Tool/software: When conducting thermal analysis, I need the Maximum Junction Temperature and Thermal Resistance parameter values. However, they are not listed in the data sheet. Can I get both values?