Part Number: TPSM33625 Other Parts Discussed in Thread: BQ25750 , Hi ,
I am finalizing the part number " TPSM33625" use as Buck converter in the BQ25750 section to use it as DRV_SUP. Input range is 11V to 26V and designing the output voltage to 10V…
Part Number: TPSM33625 Good morning,
We are using a TPSM33625 on our desing.
The expected input voltage working range is 12 to 24V and the output voltage is fixed to 3.8V.
The TPSM33625 converter supplies both a CPU SOM module and the 2.8V and 3…
Part Number: TPSM33625 Hi team, TPSM33625RDNR TPSM828211SILR I can't find the MSL level for these devices. In your web site, the MSL level is blank. Could you tell me what is the MSL level? And, why are these blank? BR, Kengo.
Part Number: TPSM33625
There's a freq setting question.
SPEC:
Vin=21.6~25.2V, Vout=12V/0.2A
According to the d/s, table8-1 it suggests Fsw=2MHz. and table8-6 suggesting Fsw=1.6Mhz for 12Vout. however, we trying to run the webench, the defalut…
Part Number: TPSM33625 Hello,
we're observing simmilar to TPSM33625: TPSM33625RDNR - Power management forum - Power management - TI E2E support forums this case behaviour. Randomly, TPSM enables into short between input and output.
Parameters input…
Part Number: TPSM33625 Tool/software: It would be very helpful to correct the datasheet accordingly, e.g. adding the information that the two SW pins should be connected together!
Kr
Part Number: TPSM33625 In earliear version of the data sheet from APR 2022 , the land pattern drawing contained via -s at pads 5 and 6 .
In the current version of data sheet SEP 2025 , the land pattern drawing DOES NOT contain via -s at pads 5 and 6…
Part Number: TPSM33625 Tool/software: The TPSM33625 part receives a single +30VDC from our product and outputs four output voltages, of which the load currents of +4V and +3.3V are 0.6A and 0.4A, respectively. First, connect each load and apply the input…
Part Number: TPSM33625 Hi Team,
I have a customer inquiry regarding the minimum input capacitance requirements for the TPSM33625.
According to the datasheet, there is a specific requirement/note for the input capacitance based on full load power calculations…
Part Number: TPSM33625 Other Parts Discussed in Thread: TPSM33620-Q1 When can we expect TPSM33625FRDNR to be back in stock? It has been designed in to an important PCB and has gone out of stock just as we enter production. On a related question on TI…