Part Number: TPSM41615 Hello Expert,
We are drawing schematic w/ this part for semiconductor tester.
We'd like to email you privately for schematic review.
Could you please send to my e-mail (michael.jeong@arrow.com)?
We will share schematic.…
Part Number: TPSM41615 Other Parts Discussed in Thread: TPSM41625
For part TPSM41625:standalone configuration
1 sync pin needs clock source matching switching frequency requirement from external source or can be left open?
2 pin 17 and 18 which…
Part Number: TPSM41615 Other Parts Discussed in Thread: TPSM41625 Hi team,
My customer is evaluating our TPSM41615 and they would like to consult with of the layout placement of TPSM41615.
For layout of TPSM41615, is it OK to place digital via under…
Part Number: TPSM41615 Hello Expert,
Our condition is Vin 12V, Vout 7V.
We would like to omptimize about Input/Output bypass capacitors.
We are drawing schmatic.
Could you please check our condition (Vin 12V, Vout 7V) and let us know recommended…
Part Number: TPSM41615 Hello Team,
My Customer is working with TPSM41615 and wanted to know how to calculate RILIM. The datasheet does not show computation. They wanted to know what RILIM value they need to set the current limit as 0.3A, 0.5A, 1.2A…
Part Number: TPSM41615 I hope to know the max. amount of units of this TPSM41615 device can parallel in interleave running condition? thanks. can it run in inteleave parallel with more than 2 units?
If it can parallel running in interleaving condtions…
Part Number: TPSM41615 Other Parts Discussed in Thread: TPSM41625 Dear Specialists,
Our customer has a question.
---
According to the datasheet P.17 7.3.8 Output On/Off Enable (EN) , it describes the EN pin has an internal pullup to BP5.
Could…
TI’s comprehensive portfolio of DC/DC switching converters and power modules absolutely features devices that can replace the regulators in the Intel® Enpirion® Power Solutions portfolio. In fact, with our advanced process and packaging technologies,…