Part Number: TPSM53604 Hi,
I will plan to use TPSM53604 for negative output. Refer to the document as below. I am no idea about the value of Cbulk. Would you help to suggest the better value of Cbulk?
www.ti.com/.../snva897
Thanks,
CC
Part Number: TPSM53604 Tool/software: WEBENCH® Design Tools Webench tool recommends a capacitor is added to the "VCC" pin which I assume is the V5V pin referenced in the datasheet, however, there is no mention of needing any form of bypass capacitor or…
Part Number: TPSM53604 Other Parts Discussed in Thread: LMZM33606 , TPSM82813 , LMZ14201 Hi I am looking for aerospace and defense grade part like TPSM53604/3/2 but current ratting should be more than 6A. Please suggest if you have any part.
Part Number: TPSM53604 Hi, I hope you are doing well right now. Our customer requested for the bxl file of TPSM53604RDAR however it is not available on our website. I would appreciate if you can share with us the bxl file for this part number. Thank you…
Part Number: TPSM53604 Hi, Could you tell me about Pin13? Pin13 names are different for Datasheet and ”EVM and Webench". Which is correct? And Are the functions different between V5V and Vcc? Regards, Yusuke
Part Number: TPSM53604 Team,
can you advise what is the spec. for Maximum Duty Cycle DMAX and Minimum ON Time tON MIN for the TPSM53604 module?
Couldn't find this in the datasheet.
Thanks for your help!
Hi Xiaoying,
I was considering TPSM13604H because the availability of TPSM53603 is poor. I hope the availability of TPSM53604 will improve
Best Regards,
Part Number: TPSM63606 Other Parts Discussed in Thread: TPSM53604 Hi Experts,
Good day.
If I want to design a positive input to provide negative output (-15V) using TPSM63606, is it possible?
I could see that PGND and AGND from its typical example of…
Part Number: BQ27542-G1 Other Parts Discussed in Thread: TPSM53604
Hello TI experts,
my customer uses battery with BQ27542 and 18650(4.2V, 3500mAh).
and they also use dummy battery in case of there is not available battery. (dummy battery is made by 12V…
Hi Harrison,
5.3V output was fed to small signal RF amplifiers through LDO's ,and the application is for CW operation.
Infact, I have tried with 4A part (TPSM53604) as well, which also shows the similar issue but at a 10.5V onwards
Thanks,
Kishore…