Part Number: TPSM5601R5 Hi,
We are experiencing an issue while simulating the TPSM5601R5 in PSpice for TI. During the simulation, we observe extremely high input current spikes, exceeding 100 A. Interestingly, we observe the same abnormal input current…
Part Number: TPSM5601R5 Hi,
We use LTspice as our primary simulation tool. Could you please provide the unencrypted SPICE model for the [TPSM5601R5]?
Thank you,
İsmet ŞEN Electrical Engineer ASELSAN
Part Number: TPSM5601R5 Tool/software: I am designing a adapter board and planning to use TPSM5601R5RDAR power module in my design. My primary requirements for the power module is , that It should be POL(Point-of-Load) Type. I went through different vendors…
Part Number: TPSM5601R5 Tool/software: Hello,
Please note the question I received from one of our customers below:
Looking at the datasheet for the TPSM5601R5 and not finding the tolerance information for the output voltage based on the FB (feedback…
Part Number: TPSM5601R5 Tool/software: I am planning on using the TPSM5601R5SRDAR power supply module to go from +24 to -15V. In the application report "Inverting Application for the TPSM5601R5H" it shows this device is capable of providing -15V. However…
Part Number: TPSM5601R5 Tool/software: Hello
On a lot of our PCB boards we have two DC-DC voltage converters to support some components with +15V and some with -15V. Our main supply voltage is +24V. the measurements were conducted at room temperature…
Part Number: TPSM5601R5 Hello TI
I have designed the TPSM5601R5 in an IBB configuration into my application.
The parameters for the circuit are 28V input voltage, -8V output voltage and max. load 0.5A.
The circuit is designed according to the…
Part Number: TPSM5601R5 Hello,
My customer is considering using the TPSM5601R5 with the following conditions.
- VIN=28V, VOUT=5V, IOUT=0.4A or 0.5A
Could you please clearfy if it is okay to use one X5R 25uF as the output capacitance?
Please let…
Part Number: TPSM5601R5 Hi Team,
Can you clarify what the actual output power of this device is, please?
The Buck modules of the TPSM5601R5 have an output power of 18W in the data sheet at the top of the features. The current rating is max.1.5A (Limit_1…
Part Number: TPSM5601R5H Other Parts Discussed in Thread: INA821 , , TPSM5601R5 , TPSM33625 Hi,
We are using the TPSM5601R5H to convert 15V to -15V. The -15V support power to 20pcs INA821 amplifiers on our board. Now we measured 105 degreeC at the top…