Part Number: TPSM560R6H Other Parts Discussed in Thread: TPSM65630 , TPSM5601R5H Hi,
I want to design a DC-DC conversion circuit using the TPSM560R6H, with an input voltage of 24V, an output voltage of -13V, and a maximum output current of 0.4A. Is…
Part Number: TPSM560R6H Other Parts Discussed in Thread: LMR36510 , LMR38010 , LMR51610 , TPSM65630 Hi,
Could you please let me know the products with low price and small package size that satisfy the following conditions?
VIN=24V, VOUT=-15V, IOUT…
Part Number: TPSM560R6H Tool/software: Hi,
I used Webench to design a DC/DC buck using the TPSM560R6H module. The input and output capacitance webench recommended is below the minimum the datasheet allows. Which is correct?
design input data:…
Part Number: TPSM560R6H Other Parts Discussed in Thread: LMR36503 , LMR36006 , TPSM365R6 , PSPICE-FOR-TI Tool/software: Hi,
We are planning to use this part in our design,but the simulation is not enabled in TI WEBENCH.
Could you please share if there…
Part Number: TPSM560R6H Tool/software: The CAD footprint provided on the TI webpage does not seem to match the datasheet specification:
Pads 1,7,8, and 14 are 0.355^mm wide - the datasheet suggests 0.5mm
The pitch between pads 6 and 7 is 0.65mm -…
Part Number: TPSM560R6H Tool/software: I'm using a TPSM560R6H in the Inverting Buck Boost topology per app note snva962. This app note, and several others pertaining to IBB topology, recommend placing a Schottky diode between -Vout and SYS_GND:
"When…
Part Number: TPSM560R6H Tool/software: Hi
Hope you are having a great day !
As per the datasheet , we need to place at least 22uF to 25uF for 10V output voltage. We have a constraint on the board space and cannot accommodate more capacitors.
Can…
Part Number: TPSM560R6H Tool/software: Hello,
We have the intention to add this DC/Dc in our project, but we have the doubt if it is necessary or not, to add an input filter in the Vin in order to block the possible conducted noise of the DC/DC. …
Part Number: TPS25751 Other Parts Discussed in Thread: TPSM560R6H We are using the TPS25751D and BQ25798RQMR a sink solution.
We like to use the solution without and with a battery of 4s.
We tested our development and could bring the PD-supply to…
Part Number: LMZM33603 Other Parts Discussed in Thread: TPSM63603 , , LM76003 , TPSM560R6H Tool/software: Hello TI Team
I am looking for a DC-DC converter with input voltage range of 12V to 32V DC, output current of 3A, with similar EMI qualification…