Part Number: TPSM5D1806 Other Parts Discussed in Thread: CSD95520 , TPS53622 , TPS546E25 , TPSM8D6C24 Tool/software: Hi Team,
May I have your suggestion for MAX20860AAFX+T replacement?
The Vin=12V and output is 0.8V/60A.
Here is the schematics since the datasheet…
Part Number: TPSM5D1806 Other Parts Discussed in Thread: , TPSM63610EVM , TPSM64406EVM , TPSM63603EVM Tool/software: Hello team,
My customer is evaluating TPSM5D1806EVM. They found the switching noise at input side increase to 0.9V when the load current…
Part Number: TPSM5D1806 Hello team,
I would like to know the soft-start time variation of dual output case. In the datasheet, the soft-start time is typical 1ms. What should be considered as the maximum and minimum soft-start time to design? almost 1ms …
The FB and VOUT waveforms definitely show the cause of the OVP, but the root cause of the OVP is elusive to me.
The ramp and clock determine the turn on and termination of the pulse width and noise can have an effect on the
switching but I have not seen…
Part Number: TPSM5D1806 I tried using the link for the webench design for the power supply listed above in dual output form. I see that the simulation is not available or supported. Could you provide SPICE models for this part? Alternatively is there…
Part Number: TPSM5D1806
Hello,
SiliconExpert Technologies has been contracted by our customer to work with their suppliers to collect component information. We would appreciate your support to provide us with the required information indicated below: …
Part Number: TPSM5D1806 Other Parts Discussed in Thread: TPS541620
Hi All,
The Device TPSM5D1806 has a pin called BP5 which as per the data sheet is a 5 V nominal (Range = 4.8 V to 5.2 V) regulated output.
My question is :
If I use Vin = 5 V, can the…
Part Number: TPSM5D1806
Hi,
There seem to be no design tools or SPICE models for this part. Also, it is not supported in Webench.
Are there plans to create a SPICE model or offer a SIMPLUS simulator to allow for more detailed analysis?
Thanks,
Jason…