Part Number: TPSM63602 HI teams,
I have one question regarding the circuit for generating negative voltage with TPSM63602RDHR. In datasheet, VLDOIN is connected to the VOUT pin (GND), but in the PSpice model, it is connected to the GND pin (VOUT), Which…
Part Number: TPSM63602 Hi TI engineers,
I encountered an issue while testing the TPSM63602V3. I observed that one half of the IC exhibits a notable temperature increase, even under no-load conditions. I've attached the schematic, thermal distribution…
Part Number: TPSM63602 Other Parts Discussed in Thread: TPSM63603EVM For the chip TPSM63602,
1. the data sheet give a recommended layout, but that does not connect the VOUT pins to the FB and VLDOIN pins,
I want to know what is the recommended approach…
Part Number: TPSM63602 Other Parts Discussed in Thread: LMZ34202 I am considering using the TPSM63602 buck converter in a system to generate 16V output based on a 36V input voltage. The TPSM6302 is rated for an input voltage range of 3V to 36V so my application…
Part Number: TPSM63602 Hi team,
On the datasheet 8.3.10 it states that VCC should be connected to AGND as below.
However, on Fig. 9-1, the VCC is connected to PGND as shown below.
Should VCC be connected to the AGND or PGND?
Best Regards,
Kei Ku…
Part Number: TPSM63606 Other Parts Discussed in Thread: TPSM63602TPSM63602, Whether it can be used produce -15vdc from a 12 v input. If possible, where can I find design tool for -ve output. and example schematic.
The Webench design tool is not allowing…
Part Number: LM22674 Other Parts Discussed in Thread: TPS5450 , TPSM63602 , TLVM13620 , TPS54061 , PTN78000H , LMR38010 , LMR51430 , LMR50410 I am working on upgrading an existing design that uses an LM22674 for a 5V supply. At low currents, 100-200mA, this…
Hello Art,
The only advice I have to share is recommend a device which has higher throughput in TI factories.
Tlvm13620 and TPSM63602 is being manufactured on a larger wafer in comparison to than older-gen devices and will be ramping across TI recently…